Hi,
Many customers of ours have mentioned that they would like the i.MX53QSB to power on automatically when power is applied. This is typical of an embedded application.
I've been told there are two iterim adjustments that could be made:
- add a transistor circuit to the front end to "push" the power on switch. I haven't looked at this in detail, but it seems a bit kludgy, and I'm wondering how well it would work as the PMIC reacts to long pushes and short pushes differently.
- "Reprogram the PMIC", this **sounds** great, and easy, except i don't think it is... Maybe first step woudl be for the board designers to provide a modified programming file.
How many people would like to see a version or a Fix/Adjustment which would allow the i.MX53 QSB to power on when power is applied? The more Votes we get, the more likely we can get this pushed up the queue of things to do.
PLEASE VOTE by replying!
Thanks,
-iain
The other option is the circuit in the attached file.
Could you post a copy of the circuit as e.g. a PNG or PDF? When I try to view the .doc, I can only see the words at the top of the page. I presume that there should be a schematic below it.
Hi all,
Later this year we expect there will be a revision of the i.MXQSB.
I just got confirmation that on this version there will be an option / instructions for a customer to have the board power on directly from plug in (i.e. no power button push necessary)
It turns out the DA9053 has an AUTO_BOOT bit with which you don’t have to wait for the on key to be grounded so the PMIC turns on, this is a bit you have to ask for it to be set since the time you order the parts and can’t be changed later, but is a good option for the customer who needs an auto wake up.
The other option is the circuit in the attached file. In case they want to test an auto wake up in the system with the QS board they can remove SW2 and add this as patch. It may not be suitable for a final application though.
Automatic power on is absolutely needed!
For every new revision of our code base for our RTOS, we are performing automatic regression tests on all of the supported targets & boards in our lab.
The procedure is usally as follow:
1. Reset the main power to the board by toggling power outlet where the AC-adapter is connected, using a remote controlled power switch.
2. Download test-software via serial/ethernet.
3. Monitor result on serial port.
This is not possible with the i.MX53QSB...
Is there a workaround available?
Regards,
Johan