Vivante drivers for Xorg version 13

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vivante drivers for Xorg version 13

859 次查看
prathameshghane
Contributor II

Hello,

We are working on i.MX6 SABRE-AUTO board.

The board is currently using the uImage built from the BSP source L3.0.35_4.1.0_130816.

We are using Xorg driver:X.Org X Server 1.12.99.905 (1.13.0 RC 5).But, The VIVANTE .so files generated using LTIB are compatible with Xorg 10.0.

We get module version mismatch error when xorg tries to load vivante modules(.so's).

Hence, we seek help regarding Vivante drivers/libraries that are compatible with Xorg 13.0 and above.

Please let us know how we can get the above mentioned libs.

Thanks and regards,

Prathamesh Ghanekar

标签 (4)
标记 (3)
0 项奖励
0 回复数