Hi,
We have designed our application board based on iMX8MQ processor. We have completed bring up of all interfaces including USB3.0 & HDMI port.
Both USB & HDMI interfaces are working fine. We are able to play saved video from USB mass storage drive to HDMI.
Now while we stream a video from Webcam USB to HDMI port. We are getting a continuous "Green screen" on HDMI 720p display and getting continuous Kernal crash logs on console. We are not able to terminate the Gstremer command using CNTL+C, the power cycle is required to do so.
See the console logs in the attached file below.
We are using below Gstreamer command:
gst-launch-1.0 v4l2src device=/dev/video2 ! 'video/x-raw,format=YUY2' ! glimagesink
Hi,
What we are changing in the kernel so that we are getting this issue in 4.14.78 but not in 4.14.98 kernel.
Is there any idea.
I want to fix this issue in 4.14.78. Is there any patch or code change available?
Thanks,
Chaitanya Sonagara
Hello,
Unfortunately, we do not have any patch to make this work. What I suggest you are to compare both drivers and see what are the difference to update in the latest kernel. Unfortunately, this is out of our scope of support.
Best regards,
Diego.
Hi Diego,
Thanks for your replay.
I tried with sync=false and waylandsink but it is not working for me.I am getting same cress.
commands are:
- gst-launch-1.0 v4l2src device=/dev/video1 ! 'video/x-raw,format=YUY2' ! glimagesink sync=false
- gst-launch-1.0 v4l2src device=/dev/video1 ! 'video/x-raw,format=YUY2' ! waylandsink
Thanks,
Chaitanya Sonagara
Hello,
I have tested with that version and I have found the problem that you encountered. However, on the L4.14.98 version, the problem is not presented. I suggest you change to that version.
I used the following pipeline.
gst-launch-1.0 v4l2src device=/dev/video2 ! 'video/x-raw,format=YUY2' ! waylandsink sync=false
Hope this may help you.
Best regards,
Diego.