Video 1080p

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Video 1080p

1,108件の閲覧回数
gerardodiiorio
Contributor I

Hi, all

the imx53 board is capable play fullhd video?

I have to choose between imx53 and beagleboardxm....

 

regards

gerardo di iorio

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

949件の閲覧回数
WangZening
NXP Employee
NXP Employee

VGA is using TVE module, the max resolution is WSXGA+(1680x1050), 60Hz.

So, you can't output 1080p through VGA port without resizing. You can resize the video and then output it to VGA. 

gerardo di iorio said:

hi, thanks for reply,

In this page https://wiki.linaro.org/Boards/MX53QuickStart  i have read what the full hd ouput is

setting  for hdmi output.

Is possible have the full hd on vga port?

In the reference manual i have read what the SATA port is SATAII with 1.5 G/s , but SATAII not is 3.0G/s?

Was is the correct speed of SATA port?

 

Regards

Gerardo Di Iorio

0 件の賞賛
返信

949件の閲覧回数
gerardodiiorio
Contributor I

hi, thanks for reply,

In this page https://wiki.linaro.org/Boards/MX53QuickStart  i have read what the full hd ouput is

setting  for hdmi output.

Is possible have the full hd on vga port?

In the reference manual i have read what the SATA port is SATAII with 1.5 G/s , but SATAII not is 3.0G/s?

Was is the correct speed of SATA port?

 

Regards

Gerardo Di Iorio

0 件の賞賛
返信

949件の閲覧回数
rlorriaux
Contributor I

Yes it does.

You can find some more documentation here: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&...

Have a look at the MMDOCS for more documentation about the codecs.

0 件の賞賛
返信