I am using the iMX8MN DDR EVK and boot the M7 core from U-Boot using the bootaux command.
I run the M7 from DDR, it is running a simple Hello World application.
I'm able to start the M7 from DDR offsets between 0x6000.0000 and higher.
However, when using a DDR offset below 0x6000.0000, the M7 does not start. Bootaux does not report an error.
All memory ranges I have tried (including those below 0x6000.0000) are not in use by U-Boot.
I know this because through 'cmp' I see the M7 binary and reserved memory is identical in all tested memory ranges before starting the M7.
M7 linker settings and U-Boot output when using DDR offset 0x8000.0000:
MEMORY
{
m_interrupts (RX) : ORIGIN = 0x80000000, LENGTH = 0x00000240
m_text (RX) : ORIGIN = 0x80000240, LENGTH = 0x0001FDC0
m_data (RW) : ORIGIN = 0x80020000, LENGTH = 0x00010000
m_data2 (RW) : ORIGIN = 0x80030000, LENGTH = 0x00010000
}
U-Boot:
imx=> mw 0x50000000 0xffffffff 0x40000
imx=> mw 0x80000000 0xffffffff 0x40000
imx=> tftp 0x50000000 test.bin
imx=> tftp 0x80000000 test.bin
imx=> dcache flush;
imx=> cmp 0x80000000 0x50000000 0x40000
Total of 262144 word(s) were the same
imx=> bootaux 0x80000000
## Starting auxiliary core stack = 0x80030000, pc = 0x80000305...
At this point, the M7 boots succesfully.
M7 linker settings and U-Boot output when using DDR offset 0x5000.0000:
MEMORY
{
m_interrupts (RX) : ORIGIN = 0x50000000, LENGTH = 0x00000240
m_text (RX) : ORIGIN = 0x50000240, LENGTH = 0x0001FDC0
m_data (RW) : ORIGIN = 0x50020000, LENGTH = 0x00010000
m_data2 (RW) : ORIGIN = 0x50030000, LENGTH = 0x00010000
}
U-Boot:
imx=> mw 0x50000000 0xffffffff 0x40000
imx=> mw 0x80000000 0xffffffff 0x40000
imx=> tftp 0x80000000 test.bin
imx=> tftp 0x50000000 test.bin
imx=> dcache flush;
imx=> cmp 0x80000000 0x50000000 0x40000
Total of 262144 word(s) were the same
imx=> bootaux 0x50000000
## Starting auxiliary core stack = 0x50030000, pc = 0x50000305...
At this point, the M7 does not boot all.
Again; I can repeat this test for various offsets with the same effect: everything above 0x6000.0000 works, e.g.
0x6000.0000, 0x8000.0000, 0xa000.0000, etc.
everything below 0x6000.0000 fails, e.g.
0x5000.0000, 0x4d00.0000, etc.
I have tested this with both my own U-Boot build, and the pre-built U-Boot from L5.4.24-2.1.0_images_MX8MNEVK.
Both give the same outcome.
According to 'i.MX 8M Nano Applications Processor Reference Manual, Rev. 0, 12/2019' the DDR ranges I use are in both the M7 and A53 memory map.
Questions:
- Am I overlooking anything that could cause this?
- Are you able to run the M7 from DDR below 0x6000.0000 on your side?
已解决! 转到解答。
Hello,
This may be due to the Arm cortex M7 processor behavior of memory access, address from 0x40000000 to 0x5FFFFFFF is used for peripheral address space and is execute never region.
While for address 0x60000000 onwards should be ok as in your test.
Hope this helps,
Best regards,
Aldo.
Hello,
This may be due to the Arm cortex M7 processor behavior of memory access, address from 0x40000000 to 0x5FFFFFFF is used for peripheral address space and is execute never region.
While for address 0x60000000 onwards should be ok as in your test.
Hope this helps,
Best regards,
Aldo.
Hi Aldo,
I see that indeed the generic ARM M7 documentation describes this as you mention.
It might be good to also mark it as such in the IMX8MNRM M7 memory map.
This explains what I'm seeing, thanks for your reply!