Hello!
I have liitle problem - image with resolution 1024x720 is good, with resolution 80x600 I see offset right side image.
I check image after IPU - it good on any resolution, I use IPU for convert input YUV422 to YUV420 and resize image.
For transfer buffer beetwen blocks (capture driver --> IPU --> VPU) I use physical addresses.
Software versions:
Linux-2.6.35.3
VPU firmware version: 1.4.41
VPU library version: 5.3.2
How can I solve this problem?
Thank you and excuse my bad english.
H264, 800x600
H264, 1280x720
Hi Kirill,
What processor are you using?
Are you using some Freescale board? If so, what?
How are you testing? Using the unit test?
Rgds
Rogerio
Hello, Rogerio!
I use our board with iMX538 CPU, it configured on 160 MHz.
My tests very simpe - save buffer before, after IPU, and after VPU, also I see result video in RTP-stream, buffer before VPU havn't this problem.
Hi BrilliantovKirillVladimirovich,
1. Every image (static or when playing video) shows this issue? Or the problem only happens when you play a video?
2. Is it possible to reproduce the problem on a Freescale board?
3. Are you using a kernel provided by Freescale? If so, where does it come from? (e.g. Freescale BSP release x.x.x, from git.freescale.com branch xxxx)
Rgds
Rogerio
Hello, Rogerio!
1. Yes, I see defect on video and static JPEG.
2. I think this will be very hard.
3. Yes, I use Linux 2.6.35.3 from BSP (L2.6.35_11.09.01_ER_source_bundle.tar.gz)
What's the display resolution? Is it always 1280x720? I mean, in both cases, is the display resolution 1280x720?
You can check it using fbset
Display resolution always FullHD (1920x1080).
How linked defect and display resolution?
Could you please send me the procedure (step by step) to reproduce the problem?
For me it's not clear what's causing the problem and I'd like to reproduce the issue.
Rgds
Rogerio
Hello, Rogerio!
1. Capture YUV422, resolution 1280x720.
2. Convert and resize YUV422 to YUV420 in IPU, output resolution 800x600.
2.1. ipu_lib_input_param_t.user_def_paddr[0] = v4l2 buffer address
ipu_lib_output_param_t.user_def_paddr[0] = codec input buffer phys addres
2.2. output resolution aligned to 16
static inline unsigned short round_size(unsigned short val,
bool to_big = false)
{
return (to_big ? (val + 15) : val) / 16 * 16;
}
3. Encode YUV420 buffer in VPU
EncOpenParam:
bitstreamBuffer 0x76a00000
bitstreamBufferSize 1638400
bitstreamFormat 2
picWidth 800
picHeight 592
frameRateInfo 65556000
bitRate 0
initialDelay 0
vbvBufferSize 0
gopSize 20
slicemode.sliceMode 0
slicemode.sliceSizeMode 0
slicemode.sliceSize 0
intraRefresh 0
sliceReport 0
mbReport 0
mbQpReport 0
rcIntraQp -1
dynamicAllocEnable 0
ringBufferEnable 0
EncStdParam.avcParam.avc_constrainedIntraPredFlag 0
EncStdParam.avcParam.avc_disableDeblk 1
EncStdParam.avcParam.avc_deblkFilterOffsetAlpha 6
EncStdParam.avcParam.avc_deblkFilterOffsetBeta 0
EncStdParam.avcParam.avc_chromaQpOffset 10
EncStdParam.avcParam.avc_audEnable 0
EncStdParam.avcParam.avc_fmoEnable 0
EncStdParam.avcParam.avc_fmoType 0
EncStdParam.avcParam.avc_fmoSliceNum 1
EncStdParam.avcParam.avc_fmoSliceSaveBufSize 32
EncParam:
enableAutoSkip 0
encLeftOffset 0
encTopOffset 0
forceIPicture 0
quantParam 10
skipPicture 0
sourceFrame 0x54ba0ea8
picStreamBufferAddr 0
picStreamBufferSize 0
Are you able to reproduce the problem using unit_tests? They're located at your rootfs /unit_tests.
I can't use it because unit_test not use IPU and work only with YUV420. This is will be not unit_test if I rewrite it for YUV422 and IPU.
>
In order to make tests, I suggest you to get the unit test that most approaches your application, modify it to meet your requirements and send me your results in case you still have problems. This way I can help to debug a possible problem on kernel or unit test code.
Rgds
Rogerio
Hello, Rogeio!
Why this is change situtation if we are use same VPU labrary?
Hi Kirill,
I'm not being able to help you because I can't see the problem on my board/system.
If you find a way to reproduce the problem on a Freescale board, use an unit test SW as base (because it will be easier for me to debug) and a clear step by step process, I can reproduce the problem and debug it. This is why I asked you to get the unit test that most approaches your application.
Rgds
Rogerio
Kirill
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
Hello, Yixing!
Unfortunally problem not soved because I can't found it reason.
Kirill
I will branch your issue into an onternal group and assign an engineer to look into it.
Regards,
Yixing