VPU issue for Android 5.0 ga using IMX6Q Sabresd board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

VPU issue for Android 5.0 ga using IMX6Q Sabresd board

跳至解决方案
839 次查看
mayqueen
Contributor IV

Hello all:

As title, I don't know why it's very slowly and no smooth when I play the video using  the source code I compiled.

But it looks okay when I use official prebuilt image (only change system.img).

I compare these two system.img, the logcat no different...

How do I fix this issue!? please help me, thanks.

标签 (2)
标记 (1)
0 项奖励
1 解答
605 次查看
igorpadykov
NXP Employee
NXP Employee

HI May

please check that you included freescale codecs in image, refer

to attached document Table 1. Freescale enhanced codecs

This document is included in IMX6_L500_100_ANDROID_DOCS 

i.MX6 Android L5.0.0_1.0.0 BSP Documentation

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
606 次查看
igorpadykov
NXP Employee
NXP Employee

HI May

please check that you included freescale codecs in image, refer

to attached document Table 1. Freescale enhanced codecs

This document is included in IMX6_L500_100_ANDROID_DOCS 

i.MX6 Android L5.0.0_1.0.0 BSP Documentation

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励