VPU issue for Android 5.0 ga using IMX6Q Sabresd board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VPU issue for Android 5.0 ga using IMX6Q Sabresd board

Jump to solution
825 Views
mayqueen
Contributor IV

Hello all:

As title, I don't know why it's very slowly and no smooth when I play the video using  the source code I compiled.

But it looks okay when I use official prebuilt image (only change system.img).

I compare these two system.img, the logcat no different...

How do I fix this issue!? please help me, thanks.

Labels (2)
Tags (1)
0 Kudos
1 Solution
591 Views
igorpadykov
NXP Employee
NXP Employee

HI May

please check that you included freescale codecs in image, refer

to attached document Table 1. Freescale enhanced codecs

This document is included in IMX6_L500_100_ANDROID_DOCS 

i.MX6 Android L5.0.0_1.0.0 BSP Documentation

Best regards

igor
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
592 Views
igorpadykov
NXP Employee
NXP Employee

HI May

please check that you included freescale codecs in image, refer

to attached document Table 1. Freescale enhanced codecs

This document is included in IMX6_L500_100_ANDROID_DOCS 

i.MX6 Android L5.0.0_1.0.0 BSP Documentation

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos