a thought but im not entirely sure is..in the init.rc file do i need to turn anything off?
import init.${ro.hardware}.usb.rc
on init
start watchdogd
# See storage config details at http://source.android.com/tech/storage/
mkdir /mnt/shell/emulated 0700 shell shell
mkdir /storage/emulated 0555 root root
export EXTERNAL_STORAGE /storage/emulated/legacy
export EMULATED_STORAGE_SOURCE /mnt/shell/emulated
export EMULATED_STORAGE_TARGET /storage/emulated
reboot
# Support legacy paths
symlink /storage/emulated/legacy /sdcard
symlink /storage/emulated/legacy /mnt/sdcard
symlink /storage/emulated/legacy /storage/sdcard0
symlink /mnt/shell/emulated/0 /storage/emulated/legacy
on boot
# Set permission for IIM node
symlink /dev/mxs_viim /dev/mxc_mem
# Set GPS serial and reset GPIO pin
setprop ro.kernel.android.gps /dev/athrnmea
setprop persist.gps.oacmode @f
symlink /dev/ttymxc2 /dev/gpsdevice
write /sys/class/gpio/export 60
write /sys/class/gpio/gpio60/direction "out"
write /sys/class/gpio/gpio60/value 1
# Enable Tethering in the Settings
setprop ro.tether.denied false
# 3D acceleration property
setprop debug.sf.showfps 0
setprop debug.sf.enable_hgl 1
setprop debug.egl.hw 1
setprop hwc.stretch.filter 1
setprop hwc.enable_dither 1
# fsl omx graphic manager media framework property
setprop media.omxgm.enable-player 1
setprop media.omxgm.enable-record 1
setprop media.omxgm.enable-scan 1
setprop rw.VIDEO_RENDER_NAME video_render.surface
#Define the config for dual camera
setprop camera.disable_zsl_mode 1
#For landscape mode, orient is 0
#For portrait mode, orient is 90
#the android before honycomb are all in portrait mode
setprop back_camera_name ov5640_mipi
setprop back_camera_orient 0
setprop front_camera_name uvc,ov5642_camera,ov5640_camera
setprop front_camera_orient 0
# Set OpenGLES version
setprop ro.opengles.version 131072
# Set rotation to 270 to cofigure as portrait mode
setprop ro.sf.hwrotation 0
# Set the density to 160dpi, default 128dpi is not good
setprop ro.sf.lcd_density 160
# change for FSL specific service
chown root system /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq
chmod 0664 /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq
chown root system /sys/devices/system/cpu/cpu0/cpufreq/scaling_min_freq
chmod 0664 /sys/devices/system/cpu/cpu0/cpufreq/scaling_min_freq
chown root system /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
chmod 0664 /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
chown root system /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_cur_freq
chmod 0440 /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_cur_freq
chown root system /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_frequencies
chown root system /sys/devices/system/cpu/cpu0/online
chmod 0664 /sys/devices/system/cpu/cpu0/online
chown root system /sys/devices/system/cpu/cpu1/online
chmod 0664 /sys/devices/system/cpu/cpu1/online
chown root system /sys/devices/system/cpu/cpu2/online
chmod 0664 /sys/devices/system/cpu/cpu2/online
chown root system /sys/devices/system/cpu/cpu3/online
chmod 0664 /sys/devices/system/cpu/cpu3/online
# prepare for ril
setprop gsm.ril.delay 15
setprop ro.ril.wake_lock_timeout 300
# Default backlight device
setprop hw.backlight.dev "pwm-backlight.0"
# Chmod/chown FSL specific sys entry
chown system system /sys/class/backlight/pwm-backlight.0/brightness
chmod 0660 /sys/class/backlight/pwm-backlight.0/brightness
# Set light sensor sysfs path and light sensor threshold lux value
setprop ro.hardware.lightsensor "/sys/class/i2c-dev/i2c-2/device/2-0044/"
setprop ro.lightsensor.threshold 20
# No bluetooth hardware present
setprop wlan.interface wlan0
# mount the debugfs
mount debugfs none /sys/kernel/debug/
service p2p_supplicant /system/bin/wpa_supplicant \
-ip2p0 -Dnl80211 -c/data/misc/wifi/p2p_supplicant.conf -N \
-iwlan0 -Dnl80211 -c/data/misc/wifi/wpa_supplicant.conf
class late_start
disabled
oneshot
service rtw_suppl_con /system/bin/rtl_wpa_supplicant \
-ip2p0 -Dnl80211 -c/data/misc/wifi/p2p_supplicant.conf -e/data/misc/wifi/entropy.bin -N \
-iwlan0 -Dnl80211 -c/data/misc/wifi/wpa_supplicant.conf
class late_start
socket wpa_wlan0 dgram 660 wifi wifi
disabled
oneshot
service wpa_supplicant /system/bin/wpa_supplicant -iwlan0 -Dnl80211
-c/data/misc/wifi/wpa_supplicant.conf
socket wpa_wlan0 dgram 660 wifi wifi
class late_start
disabled
oneshot
# magd daemon
service magd /system/bin/magd
class main
user system
group input
oneshot
# Orion InG
service ing /system/bin/ingsvcd -c /system/etc/gps/Orion.ini
socket athrkv9988 stream 666 system system
socket athrshmsocket stream 666 system system
socket athrsupl59991 stream 666 system system
class late_start
user root
group gps
oneshot
on fs
# mount ext4 partitions
mount_all /fstab.freescale