V4L2_MEMORY_USERPTR example for iMX8QM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

V4L2_MEMORY_USERPTR example for iMX8QM

Jump to solution
1,314 Views
aso
Contributor III

Hello everyone,

 

I'm programming V4L2  using Linux 4.19.35, on an evaluation board MCIMX8QM-CPU.

The camera uses MX8X MIPI4CAM2.


So the question is, is it possible to use the V4L2_MEMORY_USERPTR feature of V4L2?
Or, if you have a sample source somewhere, please let me know.

Currently, I can capture using V4L2_MEMORY_USERPTR, but when I look at the capture screen, it is black. We are currently investigating at what level the black screen is displayed.

0 Kudos
Reply
1 Solution
1,300 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply
1 Reply
1,301 Views
igorpadykov
NXP Employee
NXP Employee

Hi aso

 

one can look at unit tests example : V4L2_MEMORY_USERPTR

can be used for i.MX8M, but not with i.MX8QM:

 

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_v4l2_test/mx8_v4l2_cap_drm.c?h=imx...

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_v4l2_test/mx6s_v4l2_cap_drm.c?h=im...

 

Best regards
igor

0 Kudos
Reply