Hi
I would like to use the integrated wifi device of the i.MX8MQ EVK under linux. Afterthe boot I can see the the PCI device:
root@imx8mqevk:~# lspci -s 01:00.0 -v
01:00.0 Network controller: Qualcomm Atheros QCA6174 802.11ac Wireless Network Adapter (rev 32)
Flags: bus master, fast devsel, latency 0, IRQ 265
Memory at 18000000 (64-bit, non-prefetchable) [size=2M]
Capabilities: [40] Power Management version 3
Capabilities: [50] MSI: Enable- Count=1/8 Maskable+ 64bit-
Capabilities: [70] Express Endpoint, MSI 00
Capabilities: [100] Advanced Error Reporting
Capabilities: [148] Virtual Channel
Capabilities: [168] Device Serial Number 00-00-00-00-00-00-00-00
Capabilities: [178] Latency Tolerance Reporting
Capabilities: [180] L1 PM Substates
Kernel driver in use: hif_pci
Kernel modules: wlan
But there is no corresponding interface and iw can't detect any wifi device.
What can be wrong with my system?
Regards
Philippe
已解决! 转到解答。
Hi Philippe
one can try procedure described in sect.4.12 Wi-Fi QCA6174
attached Linux Manual and Demo Images on link
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Philippe
one can try procedure described in sect.4.12 Wi-Fi QCA6174
attached Linux Manual and Demo Images on link
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------