Hello,
We use SMSC's LAN8720A as RMII PHY on i.MX6solo and currently having problem with
send & receiving packets(Checking at U-boot).
U-Boot > ping 192.168.100.1
eth_halt: wait for stop regs
eth_halt: done
Trying FEC
fec_tbd_init
Using FEC device
fec_send: status 0x8c00 index 0 ret -22
fec_recv: ievent 0x0
fec_recv: status 0x8000
fec_recv: stop
fec_recv: ievent 0x0
fec_recv: status 0x8000
fec_recv: stop
...
First of all, normally which cause "eth_halt: wait for stop regs" at the beginning?
By looking at code, fec_send function stuck at below two points and return error codes,
while (--timeout) { | ||
if (!(readl(&fec->eth->x_des_active) & FEC_X_DES_ACTIVE_TDAR)) | ||
break; |
}
if (readw(&fec->tbd_base[fec->tbd_index].status) & FEC_TBD_READY) | |
ret = -EINVAL; |
Here's our IOMUX configuration and schematics
Needs help for fix this problem step by step.
iomux_v3_cfg_t const enet_pads[] = {
MX6_PAD_ENET_MDC__ENET_MDC | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_MDIO__ENET_MDIO | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_RXD0__ENET_RDATA_0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_RXD1__ENET_RDATA_1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_CRS_DV__ENET_RX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),
// MX6_PAD_ENET_RX_ER__ENET_RX_ER | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_RX_ER__GPIO_1_24 | MUX_PAD_CTRL(NO_PAD_CTRL),
/* FEC Intterupt */
MX6_PAD_ENET_REF_CLK__GPIO_1_23 | MUX_PAD_CTRL(NO_PAD_CTRL),
MX6_PAD_ENET_TXD0__ENET_TDATA_0 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_TXD1__ENET_TDATA_1 | MUX_PAD_CTRL(ENET_PAD_CTRL),
MX6_PAD_ENET_TX_EN__ENET_TX_EN | MUX_PAD_CTRL(ENET_PAD_CTRL),
/* clock from anatop */
MX6_PAD_GPIO_16__ENET_ANATOP_ETHERNET_REF_OUT | MUX_PAD_CTRL(ENET_PAD_CTRL),
/* LAN8720A PHY Reset */
MX6_PAD_RGMII_TXC__GPIO_6_19 | MUX_PAD_CTRL(NO_PAD_CTRL),
};
Thanks in advance,
Jay
I have exact the same issue.
TX Clock is enabled - (gpr1 bit 21 is set to 1)
Also for the ENET REF CLOCK, SION bit is enabled.
I don't understand what the issue in the dma has todo with the tx clock of the phy?
Hello Jimmy,
So far as I observe, I think yes.
U-Boot > pri ethact
ethact=FEC
U-Boot > pri ethaddr
ethaddr=00:02:BD:AB:CD:EF
U-Boot > md 021880e4 4
021880e4: 0002bdab cdef8808 00010000 00000000 ................
U-Boot > mii info
fec_mdio_read: phy: 00 reg:03 val:0xffff
fec_mdio_read: phy: 01 reg:03 val:0xc0f1
fec_mdio_read: phy: 01 reg:02 val:0x7
fec_mdio_read: phy: 01 reg:00 val:0x3100
fec_mdio_read: phy: 01 reg:05 val:0xcde1
fec_mdio_read: phy: 01 reg:00 val:0x3100
fec_mdio_read: phy: 01 reg:05 val:0xcde1
PHY 0x01: OUI = 0x01F0, Model = 0x0F, Rev = 0x01, 100baseT, FDX
If there's another way to confirm MAC address is properly configured, please let me know to do it.
Whenever I try networking relative commands like dhcp, tftpboot, nfs... etc, symptom is same as
I'd described above executing ping command.
It seems phy/mac have no clock.
so, 1. Make sure the iomux config for : MX6_PAD_GPIO_16__ENET_ANATOP_ETHERNET_REF_OUT
2. From the info from you attached, the clock is from internal anatop PLL, make sure the clock enable. You can measure the GPIO_16 PAD clock.
Thanks,
Andy
1. It's my iomux pad value
MX6_PAD_GPIO_16__ENET_ANATOP_ETHERNET_REF_OUT = IOMUX_PAD(0x05E4, 0x0214, 2, 0x080C, 0, 0),
2. Attached are measured 50Mhz clock at GPIO_16.
If it seems no problem, isn't there any other possibilities to cause the problem?
Thanks,
Jay