Using RMII(SMSC LAN8720A) on i.MX6solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using RMII(SMSC LAN8720A) on i.MX6solo

4,318 Views
jaykim
Contributor I

Hello,

We use SMSC's LAN8720A as RMII PHY on i.MX6solo and currently having problem with

send & receiving packets(Checking at U-boot).

U-Boot > ping 192.168.100.1

eth_halt: wait for stop regs

eth_halt: done

Trying FEC

fec_tbd_init

Using FEC device

fec_send: status 0x8c00 index 0 ret -22

fec_recv: ievent 0x0

fec_recv: status 0x8000

fec_recv: stop

fec_recv: ievent 0x0

fec_recv: status 0x8000

fec_recv: stop

...


First of all, normally which cause "eth_halt: wait for stop regs" at the beginning?

By looking at code, fec_send function stuck at below two points and return error codes,

while (--timeout) {
   if (!(readl(&fec->eth->x_des_active) & FEC_X_DES_ACTIVE_TDAR))
   break;

    }

if (readw(&fec->tbd_base[fec->tbd_index].status) & FEC_TBD_READY)
   ret = -EINVAL;


Here's our IOMUX configuration and schematics

Needs help for fix this problem step by step.

iomux_v3_cfg_t const enet_pads[] = {

    MX6_PAD_ENET_MDC__ENET_MDC           | MUX_PAD_CTRL(ENET_PAD_CTRL),

    MX6_PAD_ENET_MDIO__ENET_MDIO            | MUX_PAD_CTRL(ENET_PAD_CTRL),

    MX6_PAD_ENET_RXD0__ENET_RDATA_0       | MUX_PAD_CTRL(ENET_PAD_CTRL),

    MX6_PAD_ENET_RXD1__ENET_RDATA_1      | MUX_PAD_CTRL(ENET_PAD_CTRL),

    MX6_PAD_ENET_CRS_DV__ENET_RX_EN      | MUX_PAD_CTRL(ENET_PAD_CTRL),

//    MX6_PAD_ENET_RX_ER__ENET_RX_ER      | MUX_PAD_CTRL(ENET_PAD_CTRL),

    MX6_PAD_ENET_RX_ER__GPIO_1_24      | MUX_PAD_CTRL(NO_PAD_CTRL),

    /* FEC Intterupt */

    MX6_PAD_ENET_REF_CLK__GPIO_1_23      | MUX_PAD_CTRL(NO_PAD_CTRL),

    MX6_PAD_ENET_TXD0__ENET_TDATA_0      | MUX_PAD_CTRL(ENET_PAD_CTRL),

    MX6_PAD_ENET_TXD1__ENET_TDATA_1      | MUX_PAD_CTRL(ENET_PAD_CTRL),

    MX6_PAD_ENET_TX_EN__ENET_TX_EN      | MUX_PAD_CTRL(ENET_PAD_CTRL),

    /* clock from anatop */

    MX6_PAD_GPIO_16__ENET_ANATOP_ETHERNET_REF_OUT      | MUX_PAD_CTRL(ENET_PAD_CTRL),

    /* LAN8720A PHY Reset */

    MX6_PAD_RGMII_TXC__GPIO_6_19      | MUX_PAD_CTRL(NO_PAD_CTRL),

};

sch.jpg

Thanks in advance,

Jay

Labels (1)
0 Kudos
Reply
7 Replies

1,639 Views
mamsadegh
Contributor I

I have exact the same issue.

TX Clock is enabled  - (gpr1 bit 21 is set to 1)

Also for the ENET REF CLOCK, SION bit is enabled.

I don't understand what the issue in the dma has todo with the tx clock of the phy?

0 Kudos
Reply

1,639 Views
jimmychan
NXP TechSupport
NXP TechSupport

Have you set the MAC address?

Have you try to get the ip by "dhcp" command ?

Is it able to get the bootfile from server by "tftpboot" command?

0 Kudos
Reply

1,639 Views
jaykim
Contributor I

Hello Jimmy,

So far as I observe, I think yes.

U-Boot > pri ethact

ethact=FEC

U-Boot > pri ethaddr

ethaddr=00:02:BD:AB:CD:EF

U-Boot > md 021880e4 4

021880e4: 0002bdab cdef8808 00010000 00000000    ................

U-Boot > mii info

fec_mdio_read: phy: 00 reg:03 val:0xffff

fec_mdio_read: phy: 01 reg:03 val:0xc0f1

fec_mdio_read: phy: 01 reg:02 val:0x7

fec_mdio_read: phy: 01 reg:00 val:0x3100

fec_mdio_read: phy: 01 reg:05 val:0xcde1

fec_mdio_read: phy: 01 reg:00 val:0x3100

fec_mdio_read: phy: 01 reg:05 val:0xcde1

PHY 0x01: OUI = 0x01F0, Model = 0x0F, Rev = 0x01, 100baseT, FDX

If there's another way to confirm MAC address is properly configured, please let me know to do it.

Whenever I try networking relative commands like dhcp, tftpboot, nfs... etc, symptom is same as

I'd described above executing ping command.

0 Kudos
Reply

1,639 Views
DuanFugang
NXP Employee
NXP Employee

It seems phy/mac have no clock.

so, 1. Make sure the iomux config for : MX6_PAD_GPIO_16__ENET_ANATOP_ETHERNET_REF_OUT

      2. From the info from you attached, the clock is from internal anatop PLL, make sure the clock enable. You can measure the GPIO_16 PAD clock.

Thanks,

Andy

1,639 Views
jaykim
Contributor I

1. It's my iomux pad value

MX6_PAD_GPIO_16__ENET_ANATOP_ETHERNET_REF_OUT = IOMUX_PAD(0x05E4, 0x0214, 2, 0x080C, 0, 0),

2. Attached are measured 50Mhz clock at GPIO_16.

If it seems no problem, isn't there any other possibilities to cause the problem?

Thanks,

Jay

1378807149887.jpg

0 Kudos
Reply

1,639 Views
warranyu_walton
Contributor II

I'm getting the exact same problem on imx6q with a Micrel KS8721BL PHY. I also verified 50MHz clock output on the scope. Please let me know if you've find out what the issue was. Thanks.

0 Kudos
Reply

1,639 Views
EgleTeam
Contributor V

Double check on SION bit: you need to "route" 50mhz to ethernet port not only to the PHY chip.

Regards!

0 Kudos
Reply