Using MFG TOOLS with i.MX6SXSD,something wrong with it

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using MFG TOOLS with i.MX6SXSD,something wrong with it

3,443 Views
bowenzhang
Contributor II

pastedImage_1.png

log:


Allocating group tables: done                            
Writing inode tables: done                            
Creating journal (4096 blocks): done
Writing superblocks and filesystem accounting information: done

UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk3p6.
utp_poll: pass returned.
UTP: received command '$ mkfs.ext4 /dev/mmcblk3p7'
UTP: executing "mkfs.ext4 /dev/mmcblk3p7"
mke2fs 1.42.9 (28-Dec-2013)
Filesystem label=
OS type: Linux
Block size=1024 (log=0)
Fragment size=1024 (log=0)
Stride=0 blocks, Stripe width=0 blocks
2048 inodes, 8192 blocks
409 blocks (4.99%) reserved for the super user
First data block=1
Maximum filesystem blocks=8388608
1 block group
8192 blocks per group, 8192 fragments per group
2048 inodes per group

Allocating group tables: done                            
Writing inode tables: done                            
Creating journal (1024 blocks): done
Writing superblocks and filesystem accounting information: done

UTP: sending Success to kernel for command $ mkfs.ext4 /dev/mmcblk3p7.
utp_poll: pass returned.
UTP: received command '$ mount -o remount,size=600M rootfs /'
UTP: executing "mount -o remount,size=600M rootfs /"
UTP: sending Success to kernel for command $ mount -o remount,size=600M rootfs /.
utp_poll: pass returned.
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ simg2img $FILE /dev/mmcblk3p5'
UTP: executing "simg2img $FILE /dev/mmcblk3p5"
Failed to read sparse file
UTP: sending Non-success to kernel for command $ simg2img $FILE /dev/mmcblk3p5.
utp_poll: exit with status 65280

Labels (1)
6 Replies

3,224 Views
bowenzhang
Contributor II

I used demo image.Now,I have make it.because  mfg's version is wrong.thx

0 Kudos
Reply

3,224 Views
brunochen
Contributor II

Hi,

I have the same problem.

How do you know you use the wrong mfg version?

BTW, could you share how to find the correct mfg tool?

Thanks,

Bruno

0 Kudos
Reply

3,224 Views
bowenzhang
Contributor II

you  can  see the filenamepastedImage_1.png

3,224 Views
brunochen
Contributor II

Hi,

Got it. Many thanks!!!

0 Kudos
Reply

3,224 Views
bowenzhang
Contributor II

I have changed serval sd card,but nothing changed.

0 Kudos
Reply

3,224 Views
joanxie
NXP TechSupport
NXP TechSupport

could you tell me the steps? let's reproduce this, did you  use demo image or cusomized image? pls share your test steps.

0 Kudos
Reply