Use IMX8M and DVI to drive ITU-BT656

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Use IMX8M and DVI to drive ITU-BT656

911 Views
fredericduchass
Contributor III

Hello,

Is it possible to know when DVI driving ITU-BT656 will be available for IMX8M BSP ?

As far as i know it's not yet developped :

mxsfb.c\fbdev\video\drivers - linux-imx - i.MX Linux kernel 

My goal is to display using CCIR656. Maybe there is an other possibility ?

(I try using hardware like ad7610 but it doesn't work)

Thanks in advance for your answers.

Best regards

Fred

Labels (1)
0 Kudos
Reply
3 Replies

764 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fred

nxp provides drivers only for lcd boards provided with i.MX8M reference board, for example

described on below link

 Quick Start Guide for MX8-DSI-OLED1 for i.MX 8M Evaluation Kit
 Quick Start Guide for IMX-MIPI-HDMI for i.MX 8M Evaluation Kit

i.MX 8M Evaluation Kit|NXP 

Linux Release Notes document lists all supported panels

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS 

Other pannels may be supported for customers with Professional Services
NXP Professional Services|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

764 Views
fredericduchass
Contributor III

Hi Igor,

 

I don't want to use flat panel ! 

My only way to use IMX8M now is using CCIR656 output. 

 

As DVI is explained in datasheet, i believed that is was developped. But reading sourcecode, i see that its wasn't. 

Have you got a roadmap for that ??? (IMX6 support CCIR656 in the past).

0 Kudos
Reply

764 Views
igorpadykov
NXP Employee
NXP Employee

Hi Fred

not all features which are described in datasheet are supported

in software. Supported features in software can be found in linux documentation on

nxp official software page link

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

Best regards
igor

0 Kudos
Reply