We are considering move from i.MX6 Quad to i.MX6 QuadPlus, from hardware side it is pin-to-pin compatible with i.MX6 Quad/Dual.
However, on software side, we noticed that this new processor is only officially supported with Android 6.0. Now we are working with Android 5.0.1 on i.MX 6 Dual/Quad. So, if we move to QuadPlus, on software side, what should we change for that new processor?
Solved! Go to Solution.
Hi James
differences between two processors are described in EB810
i.MX 6Dual/6Quad and i.6DualPlus/6QuadPlus Applications Processor Comparison
http://cache.nxp.com/files/32bit/doc/eng_bulletin/EB810.pdf
And transfer old software may be indeed big wok, as video path is completely
different due to new modules PRE/PRG, just for reference is attached Linux
Manual, one can look at Chapter 6 Image Processing Unit (IPU) Drivers.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi James
differences between two processors are described in EB810
i.MX 6Dual/6Quad and i.6DualPlus/6QuadPlus Applications Processor Comparison
http://cache.nxp.com/files/32bit/doc/eng_bulletin/EB810.pdf
And transfer old software may be indeed big wok, as video path is completely
different due to new modules PRE/PRG, just for reference is attached Linux
Manual, one can look at Chapter 6 Image Processing Unit (IPU) Drivers.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Do We need to take care anything electrically before mounting the iMX6 Quad Plus processor in already designed iMX6 Quad PCB?
Thanks,
Tami
same thing here, we used an i.MX6duo board to mount an i.MX6duo PLUS and something goes wrong during boot process... apparently power consumption of SOC is much higher...