Update Linux Kernel (Yocto Sumo) over Ethernet for IMX8M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Update Linux Kernel (Yocto Sumo) over Ethernet for IMX8M

1,760件の閲覧回数
sourodeep_biswa
Contributor I

Hello,

We are using Dart MX8M module with Yocto Sumo and we have added some of our own custom drivers for the some camera sensor modules that we use with it.
Now we followed the procedure mentioned in 
https://variwiki.com/index.php?title=SWUpdate_Guide&release=RELEASE_SUMO_V2.2_DART-MX8M
to update the kernel over Ethernet and at step 2.4 when we upload a new software update image, we have the following error: 

Software Update started !

[extract_file_to_tmp] : Found file: filename sw-description size 412

[parse_cfg] : Version 0.1.0

[parse_hw_compatibility] : Accepted Hw Revision : 1.0

[parse_files] : Found compressed File: var-image-swupdate-imx8m-var-dart.tar.gz --> / (/dev/update)

[parse_scripts] : Found Script: update.sh

[check_hw_compatibility] : Hardware imx8m-var-dart Revision: 1.0

[check_hw_compatibility] : Hardware compatibility verified

[extract_files] : Found file: filename update.sh size 1164 required

[extract_files] : Found file: filename var-image-swupdate-imx8m-var-dart.tar.gz size 579006930 required

[network_initializer] : Valid image found: copying to FLASH

ERROR bootloader/uboot.c : bootloader_env_set : 64 : Error: environment not initialized, No such file or directory

Installation in progress

[execute_shell_script] : Calling shell script /tmp/scripts/update.sh preinst : return with 0

[install_single_image] : Found installer for stream var-image-swupdate-imx8m-var-dart.tar.gz archive

ERROR handlers/archive_handler.c : install_archive_image : 165 : Device /dev/update with filesystem ext4 cannot be mounted

[install_single_image] : Installer for archive not successful !

ERROR bootloader/uboot.c : bootloader_env_set : 64 : Error: environment not initialized, No such file or directoryInstallation failed ![network_initializer] : Main thread sleep again !Waiting for requests...

[network_initializer] : Main loop Daemon

Can anyone please help? 
Also are there any other methods of updating kernel over ethernet for Yocto? 
Any helpful links or documents are very appreciated!  


Thank you,

Best regards,
Sourodeep Biswas,

tobias.wahl@diaspective-vision.com

0 件の賞賛
返信
1 返信

1,721件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Sourodeep,

I guess this is wrong download try to download the file again, or let´s see is someone of variscite  can help?

Regards

0 件の賞賛
返信