Hi all,
My i.MX6Q Sabre Lite board is broken, because when turning it on, I have any display on the gtkterm output.
I decided to unbrick it, following this method : http://boundarydevices.com/unbricking-nitrogen6x-sabre-lite-i-mx6-board/
but when launching the imx_usb script with a u-boot.bin, I've got the following message error :
main:Could not open device vid=0x15a2 pid=0x54 err=-3
I searched on the net about this error but I couldn't find anything !!!
Does anyone have an idea, please ?
已解决! 转到解答。
Hi Albert, thanks for your answer, it has really helped me, so now I can have a U-boot on the serial console.
Trying to recover the SPI Flash, I follow this site :
i.MX6x SABRE Lite SPI Flash Recovery - Linux on ARM - eewiki
But when running the command :
MX6Q SABRELITE U-Boot > load mmc ${mmcdev}:1 0x10800000 v2013.04.imx
I have this log :
Unknown command 'load' - try 'help'
Do you have an idea ?
Do I have to run also the upgradeu command ?
Thanks in advance for your answers.
Younes
Hello,
The load commands depends on the u-boot version you are using, some has it some others don't. So maybe you should recompile a u-boot from boundary devices which should have it. Regarding the upgradeu command I don't use at all, I make everything "by hands", so I won't be able to give you advices about it. My method is this one :
* copy my u-boot to my sd card
* boot with imx_usb_loader
* copy to flash (mmc read 0x10800000 0 800 ; sf probe 1; sf erase 0 0x40000; sf write 0x10800000 0 0x40000)
* Reboot
Best regards
Hi Albert,
Thanks for your help, now when I start the board I have U-boot launching.
On my µSD card I have a kernel and rootfs from LTIB but when starting the boot, I have a memory allocation problem, you can see the log on the following:
CPU: Freescale i.MX6Q rev1.2 at 792 MHz
Reset cause: POR
Board: SABRE Lite
DRAM: 1 GiB
MMC: FSL_SDHC: 0, FSL_SDHC: 1
SF: Detected SST25VF016B with page size 4 KiB, total 2 MiB
No panel detected: default to HDMI
enable_hdmi: setup HDMI monitor
Display: HDMI (1024x768)
In: serial
Out: serial
Err: serial
Net: using phy at 6
FEC
Hit any key to stop autoboot: 0
ERROR : memory not allocated
Did I do something wrong ?
Regards
Hi Albert,
Sorry for disturbing you again, but when I switch the board to USB OTG Recovery mode, and entring the command : lsusb
I can't find the Freescale entry !!! (Tried several times ..)
I tried to launch the scrip : imx_loader anyway, but it doesn't work :smileysad:
How can I force the board to get again the freescale entry ?
Best regards
Yes of course I already did it. But now when linking the board to my computer by USB, turning the switches to USB OTG and reseting the board. Any entry named Freescale semi..... appears !!!
Now it doesn't work !!
When I turn on the board I have no display on the output serial line.
And I can't get again the Freescale entry with the lsusb command !! (Tired all the possibilities of the switches).
Well that is strange, my method to get to recovery mode is this one (I guess you're doing it well but just to check) :
* put the switch number 1 (there is two little "thing" on the switch) toward the processor and let the number 2 toward the exterior of the board.
* link by usb (OTG) the card and your computer and by serial
* boot the board and try lsusb and your computer
If it doesn't work then I don't know