Unable to use UHS SDcard in imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to use UHS SDcard in imx6

3,093件の閲覧回数
balasubramaniyam
Contributor II

Hi,

I am usig i.MX6 Processor with customize board which can support Ultra High Speed SDcard in USDHC2.

UHS-I tested in L4.9.11 kernel with Poky-Morty binaries.

supporting SDR104 in imx6 board by yocto 

From the above link I made the changes in device tree to support Ultra High Speed, but while booting SDcard failed in initialising and USDHC2 got CMD timeout error.

Changes:

&usdhc2 {
     pinctrl-names = "default", "state_100mhz", "state_200mhz";
     pinctrl-0 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_gpio>;
     pinctrl-1 = <&pinctrl_usdhc2_100mhz>, <&pinctrl_usdhc2_gpio>;
     pinctrl-2 = <&pinctrl_usdhc2_100mhz>, <&pinctrl_usdhc2_gpio>;
     cd-gpios = <&gpio4 25 GPIO_ACTIVE_LOW>;
     vmmc-supply = <&reg_sd2_vmmc>;
     keep-power-in-suspend;
     /* no-1-8-v; */
     enable-sdio-wakeup;
     status = "okay";
};

reg_sd2_vmmc: regulator@6 {
    compatible = "regulator-fixed";
     regulator-name = "P3V3_SDa_SWITCHED";
     regulator-min-microvolt = <3300000>;
     regulator-max-microvolt = <3300000>;

     /* GPIO to toggle 3.3V and 1.8V to SDcard */
     gpio = <&gpio6 11 GPIO_ACTIVE_HIGH>;
     enable-active-high;
     off-on-delay = <20000>;
};

pinctrl_usdhc2: usdhc2grp {
     fsl,pins = <
     MX6QDL_PAD_SD2_CMD__SD2_CMD 0x1F079
     MX6QDL_PAD_SD2_CLK__SD2_CLK 0x1F079
     MX6QDL_PAD_SD2_DAT0__SD2_DATA0 0x1F079
     MX6QDL_PAD_SD2_DAT1__SD2_DATA1 0x1F079
    MX6QDL_PAD_SD2_DAT2__SD2_DATA2 0x1F079
     MX6QDL_PAD_SD2_DAT3__SD2_DATA3 0x1F079
     >;
};

pinctrl_usdhc2_100mhz: usdhc2grp_100mhz {
     fsl,pins = <
     MX6QDL_PAD_SD2_CMD__SD2_CMD 0x1F079
     MX6QDL_PAD_SD2_CLK__SD2_CLK 0x1F079
     MX6QDL_PAD_SD2_DAT0__SD2_DATA0 0x1F079
     MX6QDL_PAD_SD2_DAT1__SD2_DATA1 0x1F079
     MX6QDL_PAD_SD2_DAT2__SD2_DATA2 0x1F079
    MX6QDL_PAD_SD2_DAT3__SD2_DATA3 0x1F079
     >;
};

pinctrl_usdhc2_200mhz: usdhc2grp_200mhz {
     fsl,pins = <
     MX6QDL_PAD_SD2_CMD__SD2_CMD 0x1F079
     MX6QDL_PAD_SD2_CLK__SD2_CLK 0x1F079
     MX6QDL_PAD_SD2_DAT0__SD2_DATA0 0x1F079
     MX6QDL_PAD_SD2_DAT1__SD2_DATA1 0x1F079
     MX6QDL_PAD_SD2_DAT2__SD2_DATA2 0x1F079
     MX6QDL_PAD_SD2_DAT3__SD2_DATA3 0x1F079
     >;
};

pinctrl_usdhc2_gpio: usdhc2_gpiogrp {
     fsl,pins = <
     MX6QDL_PAD_NANDF_CS0__GPIO6_IO11 0x1F088 /* PDn */
>;
};

Error log:

    

 sdhci-esdhc-imx 2194000.usdhc: Got CD GPIO
 sdhci-esdhc-imx 2194000.usdhc: change pinctrl state for uhs 0
 sdhci-esdhc-imx 2194000.usdhc: change pinctrl state for uhs 0
 mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
 sdhci-esdhc-imx 2194000.usdhc: change pinctrl state for uhs 0
 sdhci-esdhc-imx 2194000.usdhc: change pinctrl state for uhs 0
 sdhci-esdhc-imx 2194000.usdhc: change pinctrl state for uhs 0
 mmc1: error -110 whilst initialising SD card

Did I miss any entry in device tree to support Ultra high speed mode or anything?

Hoping for the better guidance.

Thanks and Regards,

Bala

ラベル(4)
タグ(4)
0 件の賞賛
返信
8 返答(返信)

2,383件の閲覧回数
balasubramaniyam
Contributor II

Hi,

We have no trouble to use UHS-I SD cards in High-Speed mode without any changes.


But once we enable 1.8V support in the device tree for Ultra-High-Speed mode the SDcard get failed in initializing and even it is not fallback to work in High-Speed mode.

And we removed pullups on the data and command lines in SDcard to test the UHS-I but the errors remain same.

0 件の賞賛
返信

2,383件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what board and bsp do you use? as I known, the latest bsp supports sd3.0 as default already, you don't change any bsp

0 件の賞賛
返信

2,383件の閲覧回数
balasubramaniyam
Contributor II

Hi Joan Xie,

I am using our customize board.

From which BSP release SD3.0 is supported?

Regards,
Bala

0 件の賞賛
返信

2,383件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

4.9.11 should support it, but you can try to use the newer version 4.9.88 without change

0 件の賞賛
返信

2,383件の閲覧回数
balasubramaniyam
Contributor II

Tested in Linux 4.9.88 kernel still behavior is same and SDcard is not working in ultra-high-speed mode.

0 件の賞賛
返信

2,383件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what board do you use? imx6Q board?

0 件の賞賛
返信

2,383件の閲覧回数
balasubramaniyam
Contributor II

imx6QP(QuadPLUS) board

0 件の賞賛
返信

2,383件の閲覧回数
jianhua_zhuang
Contributor I

can you share how to fix it?

0 件の賞賛
返信