Unable to flash imx6Q sabre sd board to emmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to flash imx6Q sabre sd board to emmc

716 Views
rizwan_s
Contributor II

Hi ,

I am working on imx6Q sabre sd board.I need to flash my binaries to emmc. when i try to flash am getting the below errors.

ModuleID[2] LevelID[1]: ../imx-3.14.28_1.0.0_ga-mfg-tools.tar\imx-3.14.28_1.0.0_ga-mfg-tools\imx-3.14.28_1.0.0_ga-mfg-tools\mfgtools-with-rootfs.tar\mfgtools-with-rootfs\mfgtools\Profiles\Linux\OS Firmware\firmware\fsl-image-mfgtool-initramfs-imx6qdlsolo.cpio.gz.u-boot failed to open.errcode is 0

ModuleID[2] LevelID[1]: Parse ucl script failed, error code: 4

It is failing during the rootfs partition.

Do i need to change anything to make it work?

Regards

Rizwan Syed

Labels (1)
0 Kudos
1 Reply

399 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rizwan

please try procedure described in attached Linux Guide

sect.4.3 Preparing an SD/MMC card to boot.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos