i.MX6 DSL DSE valure torelant

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 DSL DSE valure torelant

640 Views
toshihisasugiya
NXP Employee
NXP Employee

Hi,

We'd like to know torelant of below impedance value.

How much % varies impedance value?

IOMUXC_SW_PAD_CTL_PAD_EIM_OE_B field descriptions

Drive Strength Field

Select one of next values for pad: EIM_OE.

000 HIZ — HI-Z

001 260_OHM — 157 Ohm @ 3.3V, 260 Ohm @ 1.8V

010 130_OHM — 78 Ohm @ 3.3V, 130 Ohm @ 1.8V

011 88_OHM — 53 Ohm @ 3.3V, 88 Ohm @ 1.8V

100 65_OHM — 39 Ohm @ 3.3V, 65 Ohm @ 1.8V

101 52_OHM — 32 Ohm @ 3.3V, 52 Ohm @ 1.8V

110 43_OHM — 26 Ohm @ 3.3V, 43 Ohm @ 1.8V

111 37_OHM — 23 Ohm @ 3.3V, 37 Ohm @ 1.8V

Regards,

Sugiyama

Labels (1)
0 Kudos
2 Replies

451 Views
art
NXP Employee
NXP Employee

The tolerance of these impedance values is +/- 10%.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

451 Views
toshihisasugiya
NXP Employee
NXP Employee

Hi, Artur,

Thanks,

Sugiyama

0 Kudos