Dear I.MX community,
Am using FSL mm-codec 3.0.6 is for i.MX28 Linux L2.6.35_1.1.0_130130 release.
I need to extract the album art for the wma files which is containing album art, could anybody please let me know how this can be done suign the above BSP source
Kindly do the needful as early as possible,
Many Thanks in advance,
解決済! 解決策の投稿を見る。
in the community, you need click the "correct answer" in the bottom of the window, then the thread will be closed, thanks.
I got the SR which has the same content, I will update that, pls follow it.
Hi Guangiong Xie
As per the conversations we had in SR# 1-1306129978 : RE: SR# 1-1300515171 : Album cover extraction for wma audio files , I didn't get any replies from past many days could you Please consider this as high priority, if you are unable to share the source code ,
Could you please atleast provide the library in such a way that, wma album art data needs to be extracted & stored in an array so that I can utilize that buffer for my further processing with detailed steps
Because of this my further implementation is getting affected & delayed
Kindly do the needful as early as possible,
Eagerly awaiting for your replies,
Thanks a lot in advance,
I've replied to you in the SR, pls follow that.
and if you want to close this thread, pls click the correct answer, then we can close this thread, thanks.
Thanks a lot for your support , pls you can close this thread
Once again Many Many Thanks,
in the community, you need click the "correct answer" in the bottom of the window, then the thread will be closed, thanks.