Unable to extract Album art wma audio files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to extract Album art wma audio files

Jump to solution
1,767 Views
srinivasanshanm
Contributor III

Dear I.MX community,

Am using FSL mm-codec 3.0.6 is for i.MX28 Linux L2.6.35_1.1.0_130130 release.

I need to extract the album art for the wma files which is containing album art, could anybody please let me know how this can be done suign the above BSP source

Kindly do the needful as early as possible,

Many Thanks in advance,

Labels (3)
0 Kudos
Reply
1 Solution
1,603 Views
joanxie
NXP TechSupport
NXP TechSupport

in the community, you need click the "correct answer" in the bottom of the window, then the thread will be closed, thanks.

View solution in original post

0 Kudos
Reply
5 Replies
1,603 Views
joanxie
NXP TechSupport
NXP TechSupport

I got the SR which has the same content, I will update that, pls follow it.

0 Kudos
Reply
1,603 Views
srinivasanshanm
Contributor III

Hi Guangiong Xie

As per the conversations we had in SR# 1-1306129978 : RE: SR# 1-1300515171 : Album cover extraction for wma audio files , I didn't get any replies from past many days could you Please consider this as high priority, if you are unable to share the source code ,

Could you please atleast provide the library in such a way that,  wma album art data needs to be extracted & stored in an array so that I can utilize that buffer  for my further processing with detailed steps

Because of this my further implementation is getting affected & delayed

Kindly do the needful as early as possible,

Eagerly awaiting for your replies,

Thanks a lot in advance,

0 Kudos
Reply
1,603 Views
joanxie
NXP TechSupport
NXP TechSupport

I've replied to you in the SR, pls follow that.

and if you want to close this thread, pls click the correct answer, then we can close this thread, thanks.

0 Kudos
Reply
1,603 Views
srinivasanshanm
Contributor III

Thanks a lot for your support , pls you can close this thread

Once again Many Many Thanks,

0 Kudos
Reply
1,604 Views
joanxie
NXP TechSupport
NXP TechSupport

in the community, you need click the "correct answer" in the bottom of the window, then the thread will be closed, thanks.

0 Kudos
Reply