Unable to enable Bluetooth

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to enable Bluetooth

ソリューションへジャンプ
1,259件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

I am working on IMX8QM-MEK platform in Bluetooth. I got following error

mek_8q:/ # cat /sys/class/rfkill/rfkill0/state
1

08-16 10:41:28.795  1768  1768 D bt_upio : is_rfkill_disabled ? [0]
08-16 10:41:28.795  1768  1768 E bt_upio : set_bluetooth_power : open(/sys/class/rfkill/rfkill0/state) for write failed: Permission denied (13)

Thanks & Regards,

Vinoth S,

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
1 解決策
1,182件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

You may find it helpful to refer to the following thread where BT topic is addressed: https://community.nxp.com/message/1269459?commentID=1269459#comment-1269459 

BR,

Ivan.

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,183件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

You may find it helpful to refer to the following thread where BT topic is addressed: https://community.nxp.com/message/1269459?commentID=1269459#comment-1269459 

BR,

Ivan.

0 件の賞賛
1,182件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you Ivan for the reply.

Vinoth S,

Regards,
Vinothkumar Sekar
0 件の賞賛