Unable to download the source code for MCIMX6QAICPU2 Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to download the source code for MCIMX6QAICPU2 Board

1,796件の閲覧回数
rohitpatle
Contributor III

Hi Team,

I am trying to download the source code for MCIMX6QAICPU2 Board, while downloading i am getting below error:

$ bitbake core-image-base

WARNING: Unable to get checksum for linux-toradex SRC_URI entry defconfig: file could not be found

Parsing recipes: 100% |#######################################################| Time: 00:00:48

Parsing of 1689 .bb files complete (0 cached, 1689 parsed). 2214 targets, 163 skipped, 0 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.28.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-14.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabresd"

DISTRO            = "poky"

DISTRO_VERSION    = "2.0.1"

TUNE_FEATURES     = "arm armv7a vfp thumb neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "HEAD:dd0ba9ea4a11ab15348d4fe3574e4b28784db82f"

meta-oe          

meta-multimedia   = "HEAD:ad6133a2e95f4b83b6b3ea413598e2cd5fb3fd90"

meta-fsl-arm      = "HEAD:35b8b9bd9863de208ab60e33b55f10ee43e2619b"

meta-fsl-arm-extra = "HEAD:e200df91b70da254461c59082ddd5db0a3c415a2"

meta-fsl-demos    = "HEAD:2231e946e7a94d096394f2b2477e8184c9bbde7b"

NOTE: Preparing RunQueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

WARNING: Failed to fetch URL http://download.savannah.gnu.org/releases/quilt/quilt-0.64.tar.gz, attempting MIRRORS if available

WARNING: Failed to fetch URL http://ftp.gnu.org/gnu/m4/m4-1.4.17.tar.gz, attempting MIRRORS if available

ERROR: Fetcher failure: Fetch command failed with exit code 4, output:

wget: unable to resolve host address 'download.savannah.gnu.org'

ERROR: Function failed: Fetcher failure for URL: 'http://download.savannah.gnu.org/releases/quilt/quilt-0.64.tar.gz'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: <PATH>

ERROR: Task 18 (<PATH>/meta/recipes-devtools/quilt/quilt-native_0.64.bb, do_fetch) failed with exit code '1'

ERROR: Fetcher failure: Fetch command failed with exit code 4, output:

wget: unable to resolve host address 'ftp.gnu.org'

ERROR: Function failed: Fetcher failure for URL: 'http://ftp.gnu.org/gnu/m4/m4-1.4.17.tar.gz'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: <PATH>

ERROR: Task 1167 (/home/techmadmin/Freescale/fsl-release-bsp/sources/poky/meta/recipes-devtools/m4/m4-native_1.4.17.bb, do_fetch) failed with exit code '1'

WARNING: Failed to fetch URL git://git.sv.gnu.org/config.git, attempting MIRRORS if available

ERROR: Fetcher failure: Fetch command failed with exit code 128, output:

Cloning into bare repository '<PATH>//git2/git.sv.gnu.org.config.git'...

fatal: unable to connect to git.sv.gnu.org:

git.sv.gnu.org: Name or service not known

ERROR: Function failed: Fetcher failure for URL: 'git://git.sv.gnu.org/config.git'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in:<PATH>/x86_64-linux/gnu-config-native/20150728+gitAUTOINC+b576fa87c1-r0/temp/log.do_fetch.2517

ERROR: Task 341 (virtual:native:<PATH>/meta/recipes-devtools/gnu-config/gnu-config_git.bb, do_fetch) failed with exit code '1'

WARNING: Failed to fetch URL http://ftp.gnu.org/gnu/autoconf/autoconf-2.69.tar.gz, attempting MIRRORS if available

WARNING: Failed to fetch URL http://ftp.gnu.org/gnu/automake/automake-1.15.tar.gz, attempting MIRRORS if available

ERROR: Fetcher failure: Fetch command failed with exit code 4, output:

wget: unable to resolve host address 'ftp.gnu.org'

ERROR: Function failed: Fetcher failure for URL: 'http://ftp.gnu.org/gnu/autoconf/autoconf-2.69.tar.gz'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: <PATH>/tmp/work/x86_64-linux/autoconf-native/2.69-r11/temp/log.do_fetch.2533

ERROR: Task 314 (virtual:native:<PATH>/meta/recipes-devtools/autoconf/autoconf_2.69.bb, do_fetch) failed with exit code '1'

ERROR: Fetcher failure: Fetch command failed with exit code 4, output:

wget: unable to resolve host address 'ftp.gnu.org'

ERROR: Function failed: Fetcher failure for URL: 'http://ftp.gnu.org/gnu/automake/automake-1.15.tar.gz'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: <PATH>/x86_64-linux/automake-native/1.15-r0/temp/log.do_fetch.2546

ERROR: Task 323 (virtual:native:<PATH>/recipes-devtools/automake/automake_1.15.bb, do_fetch) failed with exit code '1'

NOTE: Tasks Summary: Attempted 7 tasks of which 0 didn't need to be rerun and 5 failed.

Please help.

Thank you,

Rohit kp

0 件の賞賛
返信
0 返答(返信)