Hi @GnasUhn!
Thank you for contacting NXP Support!
You can follow our Yocto Project User guide to install the required packages.
Install the repo utility
To get the BSP you need to have repo installed.
$ mkdir ~/bin
$ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo
$ PATH=${PATH}:~/bin
Download the Yocto Project BSP for i.MX
$ mkdir desktop
$ cd desktop
$ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-kirkstone -m imx-5.15.71-2.2.0_desktop.xml
$ repo sync
Create a new build folder
If you want to create a new build folder:
$ DISTRO=imx-desktop-xwayland MACHINE=imx8mpevk source imx-setup-desktop.sh -b build-desktop
Note: The available build MACHINEs for the below boards:
imx8mpevk - i.MX8MP-EVK
imx8mqevk - i.MX8MQ-EVK
imx8mmevk - i.MX8MM-EVK
imx8mnevk - i.MX8MN-EVK
imx8qmmek - i.MX8QM-MEK
imx8ulpevk - i.MX8ULP-EVK
imx8qxpc0mek - i.MX8QXP-MEK with silicon revision C0 chip
Use an existing build folder
If you want to build in an existing build folder:
$ cd desktop
$ source setup-environment build-desktop
Build the image for i.MX
$ bitbake imx-image-desktop
https://github.com/nxp-imx/meta-nxp-desktop
Best Regards!
Chavira
Hi, um
I followed our Yocto Project User guide, but when I used:
Build the image for i.MX
$ bitbake imx-image-desktop
I got an error:
ERROR: The following required tools (as specified by HOSTTOOLS) appear to be unavailable in PATH, please install them in order to proceed:
ar as chrpath diffstat g++ gawk gcc ld make nm objcopy objdump ranlib readelf rpcgen strings strip
Could you help me solve this error?
Hi @GnasUhn!
A Yocto Project build requires specific packages to be installed for the build that are documented under the Yocto Project. Go to Yocto Project Quick Start and check for the packages that must be installed for your build machine.
Essential Yocto Project host packages are:
$ sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential \
chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils \
iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \
python3-subunit mesa-common-dev zstd liblz4-tool file locales -y
$ sudo locale-gen en_US.UTF-8
Hi, thank you for your support, now I have enough packets for my build machine. But when I run
$ bitbake imx-image-desktop
I got some errors, so I started an NXP support case to solve them.
Thank you very much!