Hi
I'm trying to make my keyboard and mouse work so i can use the GUI of fsl-image-gui, but nothing is working.
I tried to plug the mouse only (mouse with male A cable conected to: female A to female A junction connected to: male A -> micro B cable connected to: USB OTG on the Saber Board)
Same for keyboard only (same setup)
And i also tried with a hub, but it is not better.
When i type dmesg, nothing happens when i plug in or out my mouse or my keybord.
Does the problem come from me, or from the board, i'm confused.
Thanks in advance.
PS: My keyboard is a Logitech K120
My mouse is a Logitech B100
My hub is a D-link DUB-H7
已解决! 转到解答。
Hi Philippe,
Have you tried with a OTG Cable adapter (Host)? It is because the fifth-pin on the micro-USB connector (ID) must be connected to ground when Host functionality is desired.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Philippe,
Have you tried with a OTG Cable adapter (Host)? It is because the fifth-pin on the micro-USB connector (ID) must be connected to ground when Host functionality is desired.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------