USB controller: Which field is the adress destination

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB controller: Which field is the adress destination

跳至解决方案
733 次查看
alexandredel
Contributor I

Hello

I'm working on the USB controller of the IMX 6Quad and i don't understand something. I read the documentation named "Application Processor Reference Manual", chapter 65, page 5270, but i don't find which field set up the adress destination for an iTD.

Is it the buffer pointer? Does someone knows this information? Or can help me to find it?

Thanks

Alexandre

标签 (1)
0 项奖励
回复
1 解答
643 次查看
Yuri
NXP Employee
NXP Employee

Yes, - the buffer pointer.

Note, new Reference Manual release (IMX6DQRM, Rev 2, 06/2014) is available now.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
644 次查看
Yuri
NXP Employee
NXP Employee

Yes, - the buffer pointer.

Note, new Reference Manual release (IMX6DQRM, Rev 2, 06/2014) is available now.

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复