Hi Community,
This is similar to https://community.freescale.com/thread/328781
(UAC2 does not work on i.MX6SL EVK)
My environment is:
-- Hardware: iMX6SL EVK, connect EVK OTG port to Ubuntu 12.04 LTS USB Host
-- Software: Freescale's 3.10.17-1.0.0 Yocto BSP (branch imx-3.10.17-1.0.0_ga)
-- repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.10.17-1.0.0_ga
-- How I build:
-- Enable CONFIG_GADGET_UAC1, CONFIG_USB_AUDIO in "arch/arm/configs/imx_v7_defconfig"
-- export MACHINE=imx6slevk; source setup-environment build
-- bitbake fsl-image-test
-- Host PC is Ubuntu 12.04 LTS
Serial message from i.MX6SL EVK is:
root@imx6slevk:~# modprobe g_audio
g_audio gadget: Hardware params: access 3, format 2, channels 2, rate 48000
g_audio gadget: audio_buf_size 48000, req_buf_size 200, req_count 256
g_audio gadget: Linux USB Audio Gadget, version: Feb 2, 2012
g_audio gadget: g_audio ready
root@imx6slevk:~# g_audio gadget: high-speed config #1: Linux USB Audio Gadget
g_audio gadget: ep1out queue req: err = -22
g_audio gadget: ep1out queue req: err = -22
We have the same issue on Wandboard Solo, Wandboard Quad too.
Any suggestions? Did anyone get UAC1 work on any iMX6 platform?
Thank you very much.
已解决! 转到解答。
Karina and Adeneo Engineering Team,
I fixed the Windows 7 issue and get UAC1 working with Windows 7 host.
Thanks for your looking into this issue.
The remaining issue is that EVK (with UAC1) can NOT get detected by Windows 7 Host, after "modprobe g_audio"
I post a question to linux-usb mailing list, with message as below:
--------------------------------------------
Subject: [linux-usb] USB Gadget drivers Windows 7/8 support and .bAlternateSetting in interface descriptor
Hi Community,
My environment is Freescale i.MX6SL EVK board (as USB peripheral device), which is based on kernel 3.10.17. i.MX6SL uses ChipIdea dual-role controller.
My problem is that gadget drivers g_ether and g_audio (UAC1 enabled) can NOT be detected by Windows 7 natively, while g_mass_storage, g_serial, g_hid can be detected by Windows 7 natively.
1) I found that both Ether and USB Audio uses .bAlternateSetting, while Mass Storage, Serial and HID do NOT. I am wondering if this is related to how Gadget framework handles USB_REQ_SET_INTERFACE request?
2) Also, I am not sure if it is related to ChipIdea quirk (gadget_supports_altsettings in file gadget_chips.h)?
Any suggestions / comments on this? Thanks.
--
Thanks,
Xuebing Wang
--------------------------------------------
Fabio,
Yes, we need to apply kernel patches. I am planning to fix other UAC1 issues, and then submit patch set to you to upstream. Is it ok?
The issues I observed now:
1) Warning message "ci_hdrc ci_hdrc.0: enabling a non-empty endpoint!", this results in 2 real problems. i) can not playback from Ubuntu 12.04 LTS 2) on Mac, can not play again after stop playing.
2) Volume control?
3) Add Mic capture
4) Other issues I am going to describe in detail in my patchset
Xuebing,
I can help you with the uspstream process, but as suggested in the linux-usb list:
http://www.spinics.net/lists/linux-usb/msg112207.html
,please run the tests on 3.16.1 or 3.17-rc.
Regards,
Fabio Estevam
Xuebing,
The mainline kernel can be installed from kernel.org.
What I meant (and the other folks at linux-usb) is that you should use the latest kernel and provide patches against it, so your patches could be reviewed in the linux-usb list and then applied into the kernel.
Fabio,
I understand. And sorry I might be unclear.
My question is: how can I get mainline kernel running on i.MX6SL EVK (or my Wandboard), thus I can run the test of UAC1 on different Host before submitting for review?
Thanks.
git clone git://git.kernel.org/pub/scm/linux/kernel/git/stable/linux-stable.git
Create a local branch based om 3.16
make imx_v6_v7_defconfig
make
make imx6sl-evk.dtb
I managed to get i.MX6SL EVK (for UAC1) detected by Linux and Mac with below patch after "modprobe g_audio"
From: Xuebing Wang <xbing6@gmail.com>
Date: Sun, 17 Aug 2014 11:06:04 +0800
Subject: [PATCH] UAC1: Enable CONFIG_GADGET_UAC1 and fix the -22 in
f_audio_set_alt issue
Error message from serial console is:
g_audio gadget: ep1out queue req: err = -22
Signed-off-by: Xuebing Wang <xbing6@gmail.com>
---
arch/arm/configs/imx_v7_defconfig | 1 +
drivers/usb/gadget/f_uac1.c | 2 ++
2 files changed, 3 insertions(+)
diff --git a/arch/arm/configs/imx_v7_defconfig b/arch/arm/configs/imx_v7_defconfig
index 4c47406..d312f7b 100644
--- a/arch/arm/configs/imx_v7_defconfig
+++ b/arch/arm/configs/imx_v7_defconfig
@@ -249,6 +249,7 @@ CONFIG_USB_PHY=y
CONFIG_NOP_USB_XCEIV=y
CONFIG_USB_MXS_PHY=y
CONFIG_USB_GADGET=y
+CONFIG_GADGET_UAC1=y
CONFIG_USB_AUDIO=m
CONFIG_USB_G_HID=m
CONFIG_USB_ZERO=m
diff --git a/drivers/usb/gadget/f_uac1.c b/drivers/usb/gadget/f_uac1.c
index fa8ea4e..a4e8e30 100644
--- a/drivers/usb/gadget/f_uac1.c
+++ b/drivers/usb/gadget/f_uac1.c
@@ -544,6 +544,7 @@ static int f_audio_set_alt(struct usb_function *f, unsigned intf, unsigned alt)
{
struct f_audio *audio = func_to_audio(f);
struct usb_composite_dev *cdev = f->config->cdev;
+ struct usb_gadget *gadget = cdev->gadget;
struct usb_ep *out_ep = audio->out_ep;
struct usb_request *req;
int i = 0, err = 0;
@@ -553,6 +554,7 @@ static int f_audio_set_alt(struct usb_function *f, unsigned intf, unsigned alt)
if (intf == 1) {
if (alt == 1) {
usb_ep_enable(out_ep);
+ config_ep_by_speed(gadget, f, out_ep);
out_ep->driver_data = audio;
audio->copy_buf = f_audio_buffer_alloc(audio_buf_size);
if (IS_ERR(audio->copy_buf))
--
2.0.1
With above patch, I still can NOT hear sound at i.MX6SL EVK.
After using UAC2 mechanism for handling ALSA sound card part, then I can hear sound after connecting EVK to both Linux and Mac. The patchset of using UAC2 sound card mechanism is too big to be posted here.
Hi Xuebing,
Currently, I'm using SabreSD based custom board with Yocto3.10.17.
I'm also facing the issue in UAC2 like,
ci_hdrc ci_hdrc.0: request length too big for isochronous
snd_uac2 snd_uac2.0: 1116 Error!
Please share your patch or code or knowledge to Fix this issue.
I put SR for the same but no reply from freescale side.
Thanks in Advance.
J.P.Raja