USB OTG2 host mode VBUS toggles continuously

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB OTG2 host mode VBUS toggles continuously

1,046件の閲覧回数
prabhatkumar
Contributor II

Hi,

In host mode, custom board USB OTG port detects the device and the USB_OTG2_ID pin goes low but the USB_OTG2_PWR pin from CPU is toggling from 0V to 3.2V continuously whenever a device (flash drive) is connected to the host. I checked USB_OTG2_OC pin and there is no over current issue either.

Can someone please explain why USB_OTG2_PWR continuously toggles when the board is in host mode?

Thanks

ラベル(6)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

779件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Prabhat

this looks like board hardware/layout error, as
USB_OTG2_PWR is connected on i.MX6UL EVK (SPF-28617.PDF)
to GPIO_2 pad and its power domain NVCC_GPIO can not exceed
datasheet requirements 3.6V, defined in Table 11. Operating Ranges i.MX6UL Datasheet
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6ULCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

779件の閲覧回数
prabhatkumar
Contributor II

Hi Igor,

My apologies, it is toggling between 0 and 3.2V. USB_OTG2_PWR is connected to A16 (ENET2_TX_DATA1) pin and it is operating in ALT8 mode. According to the datasheet, It should work as well when connected to ENET2_TX_DATA1 pad.

0 件の賞賛
返信