Dear community.
Our customer has question below.
When using OTG port of USB Function in i.MX6DL , there is a problem that the cutoff measure when disconnect USB Host device is slow.
When the source cord was confirmed, it was the following cord.
It's defined as 155ms-200ms on Spec in USB OTG defined by usb.org, but their system is 500ms setting.
I think there is no problem even in the 155ms according to the Spec. Or it will become a problem because it is set to 500ms in the relationship of the electrical characteristics of i.MX6.
[Source cord]
/* B-Idle to A-Disconnect */
#define TA_BIDL_ADIS (500) /* TA_BIDL_ADIS: section 5.2.1
* 155ms ~ 200 ms (but not enough)
*/
解決済! 解決策の投稿を見る。
Hi Takashi,
I have internally escalated your request and below you can find the summarized reply:
The B_IDLE to A_DISCONNECT is an OTG specification and applies only to OTG role change. Is that what you are trying to do? i.e. role change without disconnecting the cable?
The problem is likely that there is some capacitance on the VBUS signal that keeps its charge too long and thus it takes a long time before the disconnection is detected.
There is a resistor in the PHY that can be enabled to discharge VBUS. This resistor can be enabled with the VD bit (bit 0) in the USB_OTGSC register. Software can enable this bit after the controller reported SUSPEND. If VBUS is at 5V it will draw some 8 mA. If the cable is disconnected, the VBUS voltage will drop quickly (depending on the Vbus cap) and if the cable is not disconnected, VBUS will remain at its level. Therefore, the resistor should be disabled when a disconnection is detected or after a timeout when the cable is not disconnected.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Takashi,
I have internally escalated your request and below you can find the summarized reply:
The B_IDLE to A_DISCONNECT is an OTG specification and applies only to OTG role change. Is that what you are trying to do? i.e. role change without disconnecting the cable?
The problem is likely that there is some capacitance on the VBUS signal that keeps its charge too long and thus it takes a long time before the disconnection is detected.
There is a resistor in the PHY that can be enabled to discharge VBUS. This resistor can be enabled with the VD bit (bit 0) in the USB_OTGSC register. Software can enable this bit after the controller reported SUSPEND. If VBUS is at 5V it will draw some 8 mA. If the cable is disconnected, the VBUS voltage will drop quickly (depending on the Vbus cap) and if the cable is not disconnected, VBUS will remain at its level. Therefore, the resistor should be disabled when a disconnection is detected or after a timeout when the cable is not disconnected.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Carlos.
Thank you for your kindly answer.
I was able to understand the mechanism of USB OTG cut off time by your description.
There are described in the following link to check the i.MX6 BSP "imx_3.10.53_1.1.0_ga" of NXP, Inc., it had been implemented in 160ms in the source code of the BSP.
Customers will probably be used in the latency of 160m
Line 40:
/ * B-Idle to A-Disconnect * /
#define TA_BIDL_ADIS (160) / * TA_BIDL_ADIS: section 5.2.1
* 155ms ~ 200 ms
* /
Thank you,
Best Regards.
T.Takahashi.