USB OTG IMX8MPlus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,902件の閲覧回数
ChienNQ
Contributor II

How to design USB micro for IMX8MPlus?

How to Implement usb otg without USB ID? 

I did not find the ID pin on the IMX8Mplus, on the datassheet documentation, please support? Can i use any GPIO for detect function? 

0 件の賞賛
返信
1 解決策
1,772件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @ChienNQ,

USB1_ID pin muxing is available on GPIO1_IO10 only. One can check the same from the Config Tools for i.MX Applications Processors.

Thanks & Regards,
Ritesh M Patel

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
1,864件の閲覧回数
ChienNQ
Contributor II

Thanks for great support

0 件の賞賛
返信
1,876件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @ChienNQ,

I hope you are doing well.

The USBx_ID is muxed with GPIO. One can refer to Page 1350 of i.MX8MP Reference Manual.
USB1_ID --> GPIO1_IO10
USB2_ID --> GPIO1_IO11

To implement the USB OTG functionality without USB-C, one can refer to the below-mentioned link which is valid for i.MX8MP as well.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-i-MX8MQ-USB2-0-Design-Without-US...

I hope it helps.

Thanks & Regards,
Ritesh M Patel

1,808件の閲覧回数
ChienNQ
Contributor II

Hi @riteshmpatel ,

Thanks for support. 

We build our device form compulab SOM UCM-iMX8PLUS . 

And they did not connect GPIO1_IO10 to SOM. Can i use another GPIO like GPIO1_0 for ID function?

Please see this link for more detail https://www.compulab.com/wp-content/uploads/2022/03/ucm-imx8plus_reference-guide_2023-01-12.pdf

Thanks and best regards,

 

0 件の賞賛
返信
1,773件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @ChienNQ,

USB1_ID pin muxing is available on GPIO1_IO10 only. One can check the same from the Config Tools for i.MX Applications Processors.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信
1,726件の閲覧回数
ChienNQ
Contributor II

Hi @riteshmpatel ,

Thanks for support us. 

One more question, in case IMX8MP Plus is in bootloader mode, is it always in device mode? and regardless of the state of the ID?

Thanks and best regards,

Trend Nguyen

0 件の賞賛
返信
1,859件の閲覧回数
khang_letruong
Senior Contributor III
0 件の賞賛
返信
1,798件の閲覧回数
ChienNQ
Contributor II

Thanks @khang_letruong 

0 件の賞賛
返信