USB Communication between to self powered boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Communication between to self powered boards

807件の閲覧回数
DSEngineer
Contributor I

Hi Everyone,
I'm working on a design and I'm not sure it will work properly.
Mainly because the USB is OTG and there is no VBUS connection between the boards.
I want to make a connection between two boards, each board has it's own power supply, there is no VBUS connection between the boards. One board will function as a master and the other as a device.
Does anyone have suggestions for repair/addition or advice on how to do it better?
I added a picture to illustrate the connection between the boards.

ラベル(1)
0 件の賞賛
3 返答(返信)

786件の閲覧回数
DSEngineer
Contributor I

Hi Igor,
Thanks for the help.
Yes, I was thinking about this configuration, but when one is set as a device he does not expect to get 5V in VBUS? Will there be a VBUS on the side of the device or will I have to connect the VBUS directly to 5V?

0 件の賞賛

784件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>Will there be a VBUS on the side of the device or will I have to connect the VBUS directly to 5V?

 

on device side VBUS can be connected directly to 5V.

 

Best regards
igor

0 件の賞賛

795件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Daniel

 

for communication between two boards one can try to use usb unit tests, configure

one board as host other as device:

https://source.codeaurora.org/external/imx/imx-test/tree/test/mxc_usb_test?h=lf-5.10.52_2.1.0

 

Best regards
igor

0 件の賞賛