I have a custom board loosely based off the i.MX53 QSB with a dedicated USB client port. I am trying to get USB client functionality working in mainline u-boot 2015.04. I have verified that USB client/gadget functionality works when booted into Linux on the board. In u-boot I have tried testing USB client with USB Mass Storage, DFU, and FastBoot and none of them seem to work.
Here is my USB client #defines from my config header file:
#define CONFIG_CI_UDC
#define CONFIG_USBD_HS
#define CONFIG_USB_GADGET_DUALSPEED
#define CONFIG_USB_GADGET
#define CONFIG_CMD_USB_MASS_STORAGE
#define CONFIG_USB_GADGET_MASS_STORAGE
#define CONFIG_USBDOWNLOAD_GADGET
#define CONFIG_USB_GADGET_VBUS_DRAW 2
#define CONFIG_USB_ETHER
#define CONFIG_USB_ETH_CDC
#define CONFIG_G_DNL_VENDOR_NUM 0x0525
#define CONFIG_G_DNL_PRODUCT_NUM 0xa4a5
#define CONFIG_G_DNL_MANUFACTURER "FSL"
#define CONFIG_SYS_CACHELINE_SIZE 64
When I run the 'ums 0 mmc 0' command, I get the following:
UMS: disk start sector: 0x0, count: 0xe88000
and then I get an infinite spinning progress indicator. At this point when I connect the USB cable to a Host PC, I see nothing on the host PC side (Windows or Liunx).
Any ideas on what I am missing to get USB client working or any hints on how to debug this further.
已解决! 转到解答。
I looks like the current i.MX5x USB support in u-boot 2015.04 only supports one USB port at a time. To enable support for the USB OTG port, you would need to use the following line in the board configuration header:
#define CONFIG_MXC_USB_PORT 0
To enable support for the first USB Host port, the following line in the board configuration header is needed:
#define CONFIG_MXC_USB_PORT 1
Hi Matthew,
This is how I got ums working on the imx6 warp board:
git.denx.de Git - u-boot/u-boot-imx.git/commitdiff http://git.denx.de/?p=u-boot/u-boot-imx.git;a=commitdiff;h=09ac7b5961396ffb8644e180180b33008e0b6b35
Maybe you missed board_usb_phy_mode().
int board_usb_phy_mode(int port)
{
if (port == 1)
return USB_INIT_HOST;
else
return USB_INIT_DEVICE;
}
Regards,
Fabio Estevam
Fabio,
I did not have a board_usb_phy_mode() function in my board file. I added one like how you implemented it and tried again. I am getting the same results as before with no response from the host PC.
Here is my board file content related to USB:
#ifdef CONFIG_USB_EHCI_MX5
static void setup_usb(void)
{
imx_iomux_v3_setup_pad(MX53_PAD_GPIO_0__GPIO1_0);
}
int board_ehci_hcd_init(int port)
{
/* Enable USB_H1_VBUS power with GPIO1_0 */
gpio_direction_output(IMX_GPIO_NR(1, 0), 1);
return 0;
}
#endif
int board_usb_phy_mode(int port)
{
if (port == 1)
return USB_INIT_HOST;
else
return USB_INIT_DEVICE;
}
Then later on in board_init(), I have:
#ifdef CONFIG_USB_EHCI_MX5
setup_usb();
#endif
Additionally here are my #defines for the USB host functionality:
/* USB Host Configs */
#define CONFIG_CMD_USB
#define CONFIG_USB_EHCI
#define CONFIG_USB_EHCI_MX5
#define CONFIG_USB_STORAGE
#define CONFIG_USB_HOST_ETHER
#define CONFIG_USB_ETHER_ASIX
#define CONFIG_USB_ETHER_MCS7830
#define CONFIG_USB_ETHER_SMSC95XX
#define CONFIG_MXC_USB_PORT 1
#define CONFIG_MXC_USB_PORTSC (PORT_PTS_UTMI | PORT_PTS_PTW)
#define CONFIG_MXC_USB_FLAGS 0
Anything else that I can try out?
Regards,
Matthew Starr
I looks like the current i.MX5x USB support in u-boot 2015.04 only supports one USB port at a time. To enable support for the USB OTG port, you would need to use the following line in the board configuration header:
#define CONFIG_MXC_USB_PORT 0
To enable support for the first USB Host port, the following line in the board configuration header is needed:
#define CONFIG_MXC_USB_PORT 1