UART serial port missing on IMX8QM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART serial port missing on IMX8QM

ソリューションへジャンプ
360件の閲覧回数
Lincoln_Dessen
Contributor II

Hi all,

 After I add two more pin configs in `arch/arm64/boot/dts/freescale/fsl-imx8qm-mek.dtsi` file:

Lincoln_Dessen_1-1687855353141.pngLincoln_Dessen_2-1687855381763.png

uart3 serial port ttyLP3 is missing in /dev:

Lincoln_Dessen_0-1687855259218.png

# dmesg | grep tty:

Lincoln_Dessen_3-1687855563041.png

 

 ttyLP3 only shows up If I remove GPIO0_IO03 and GPIO0_IO04 configs. 

Is there something wrong with my gpio setting in dts file? 

 

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
346件の閲覧回数
Lincoln_Dessen
Contributor II

It seems the cause is I configure the same pin twice on different places.  

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
347件の閲覧回数
Lincoln_Dessen
Contributor II

It seems the cause is I configure the same pin twice on different places.  

0 件の賞賛
返信