Hi,
Actually i am new to Linux kernel and u-boot.Ours is a custom board based on i.Mx6 and there is need for configuring UART (1,2,3,4) but i am not sure how to configure all the UART ports for our custom board .so Can anyone help me configuring the UART for the Linux Kernel .
Thank you,
Deepanraj.A
Hi Deepanraj.A,
Here I give you a document Debug UART Customization on i.MX6x.ppt which you can refer to configure the uart. Hope this can help you.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
Have you received Debug UART Customization on i.MX6x.ppt by now? If not, contact me.
Have a great day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
But Actually i wanted to configure my serial UART3 in the speed of 4000000 so not the debug UART.Debug UART useing it as it is.So is there any way to configure other usart at speed of 4000000.
Hi Deepanraj.A,
About the configure of uart you can refer to document i.MX_6Dual6Quad_Linux_Reference_Manual.pdf. You can see the source code under directory <ltib_dir>/rpm/BUILD/linux/drivers/tty/serial. Details are in this document. Hope this can help you.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Deepanraj,
You can go to the directory <ltib_dir>/rpm/BUILD/linux/drivers/tty/serial in your BSP source code, you can see the file imx.c, there are configurations for UART.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Did you ever get this resolved?
I understand you're leaving the debug UART as is (for debugging) are you/have you implemented access to all other UARTs?
Appreciate any issues you ran into that I might avoid!
Thanks,
mike
Hi Mike
Actually i have figured how to configure the UART at 4Mbps now.But my problem is that when i configure the UART3 & UART4 at 4Mbps i am not able to configure other two UART1 & UART5 at 115200bps since all the UART are configured at 4Mbps
Thank you,
Deepanraj.A
Hmmmmmmmm....That is odd.
I have not encountered this type of behavior. Without eyeballing everything it's difficult to point somewhere!
I would recommend going back to the start, assume nothing, review the HW and pin-out connectivity to where you are measuring. Then move on to review IOMUX settings to ensure there are no errors - and finally in the kernel init.c make sure you all is in order. Typically I've found that something simple is staring you in the face while you look hard for deeper complexities.
mike
Hi Deepanraj.A,
I have attached it in my last reply to you. And I can see it now really in the reply. You can have a check. You'd better go to the thread link to see it, not in inbox. The thread link is https://community.freescale.com/thread/329949, if you still can not find it, tell me easily. I will attached it for you again.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Deepanraj
you can check Chapter 3 "Registering a New UART Driver"
i.MX_6Dual6Quad_BSP_Porting_Guide.pdf included in
Best regards
chip