UART RX interrupt loop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART RX interrupt loop

ソリューションへジャンプ
2,633件の閲覧回数
andyteufel
Contributor III

Hello,

I am trying to get UART running with EDMA on an MIMXRT1010. The problem I have is that once a "Receive Data Register Full" interrupt is triggered, the interrupt "gets stuck" and the interrupt handler is executed in a loop, even though nothing is being received anymore. Clearing the interrupt and status flags does not help.

This is what my interrupt handler looks like:

void LPUART1_IRQHandler(void) {
    log_info("IRQ: Status flags 0x%08X, FIFO flags 0x%08X", LPUART1->STAT, LPUART1->FIFO);
    if (LPUART_GetStatusFlags(LPUART1) & kLPUART_RxDataRegFullFlag) {
        uint8_t data = LPUART_ReadByte(LPUART1);
        log_info("UART RX: %02X", data);
    }
    NVIC_ClearPendingIRQ(LPUART1_IRQn); // This does not help
    SDK_ISR_EXIT_BARRIER;
}

 With that I get the following in the logs:

IRQ: Status flags 0x01E2C000, FIFO flags 0x00800099
UART RX: 00
IRQ: Status flags 0x01C2C000, FIFO flags 0x00C00099
IRQ: Status flags 0x01C2C000, FIFO flags 0x00C00099
... (continues)

 

This is basically starving my application since the only thing that's running anymore is this interrupt handler. What am I doing wrong?

This is the UART initialization code:

#define BLUETOOTH_UART_RX_IOMUX             IOMUXC_GPIO_09_LPUART1_RXD
#define BLUETOOTH_UART_TX_IOMUX             IOMUXC_GPIO_10_LPUART1_TXD

#define BLUETOOTH_UART_PORT                 LPUART1
#define BLUETOOTH_UART_IRQn                 LPUART1_IRQn
#define BLUETOOTH_UART_BAUDRATE             115200u

#define LPUART_TX_DMA_CHANNEL               0u
#define LPUART_TX_DMA_REQUEST               kDmaRequestMuxLPUART1Tx
#define BT_LPUART_DMAMUX_BASEADDR           DMAMUX
#define BT_LPUART_DMA_BASEADDR              DMA0

void board_hal_uart_init(const board_hal_uart_config_t *p_config) {
    APP_ASSERT(p_config != NULL, "Invalid UART configuration");
    APP_ASSERT(p_config->rx_isr_handler != NULL, "Invalid UART RX ISR handler");
    APP_ASSERT(p_config->tx_done_callback != NULL, "Invalid UART TX done callback");
    m_bluetooth_uart.p_config = p_config;

    IOMUXC_SetPinMux(BLUETOOTH_UART_RX_IOMUX, 0u);
    IOMUXC_SetPinMux(BLUETOOTH_UART_TX_IOMUX, 0u);

    IOMUXC_SetPinConfig(BLUETOOTH_UART_RX_IOMUX, GPIO_SLEW_RATE_CONFIG(GPIO_SLEW_RATE_SLOW) |
                                                 GPIO_DRIVE_STRENGTH_CONFIG(GPIO_DRIVE_STRENGTH_R04) |
                                                 GPIO_SPEED_CONFIG(GPIO_SPEED_FAST_150MHz) |
                                                 GPIO_OPEN_DRAIN_CONFIG(GPIO_OPEN_DRAIN_ENABLED) |
                                                 GPIO_PULLKEEP_CONFIG(GPIO_PULLKEEP_DISABLED) |
                                                 GPIO_PULLKEEP_SELECT_CONFIG(GPIO_PULLKEEP_SELECT_KEEPER) |
                                                 GPIO_PULL_CONFIG(GPIO_PULL_PU_22KOhm) |
                                                 GPIO_HYSTERESIS_CONFIG(GPIO_HYSTERESIS_DISABLED));

    IOMUXC_SetPinConfig(BLUETOOTH_UART_TX_IOMUX, GPIO_SLEW_RATE_CONFIG(GPIO_SLEW_RATE_SLOW) |
                                                 GPIO_DRIVE_STRENGTH_CONFIG(GPIO_DRIVE_STRENGTH_R04) |
                                                 GPIO_SPEED_CONFIG(GPIO_SPEED_FAST_150MHz) |
                                                 GPIO_OPEN_DRAIN_CONFIG(GPIO_OPEN_DRAIN_ENABLED) |
                                                 GPIO_PULLKEEP_CONFIG(GPIO_PULLKEEP_DISABLED) |
                                                 GPIO_PULLKEEP_SELECT_CONFIG(GPIO_PULLKEEP_SELECT_KEEPER) |
                                                 GPIO_PULL_CONFIG(GPIO_PULL_PU_22KOhm) |
                                                 GPIO_HYSTERESIS_CONFIG(GPIO_HYSTERESIS_DISABLED));

    lpuart_config_t uart_config;
    LPUART_GetDefaultConfig(&uart_config);
    uart_config.baudRate_Bps = BLUETOOTH_UART_BAUDRATE;
    uart_config.enableRx     = true;
    uart_config.enableTx     = true;

    status_t status = LPUART_Init(BLUETOOTH_UART_PORT, &uart_config, board_hal_uart_get_frequency());
    APP_ASSERT(status == kStatus_Success, "Failed to initialize UART");

    LPUART_EnableInterrupts(BLUETOOTH_UART_PORT, kLPUART_RxDataRegFullInterruptEnable);
    NVIC_SetPriority(LPUART1_IRQn, BLUETOOTH_UART_INTERRUPT_PRIORITY);
    EnableIRQ(BLUETOOTH_UART_IRQn);

#if defined(FSL_FEATURE_SOC_DMAMUX_COUNT) && FSL_FEATURE_SOC_DMAMUX_COUNT
    DMAMUX_Init(BT_LPUART_DMAMUX_BASEADDR);
    DMAMUX_SetSource(BT_LPUART_DMAMUX_BASEADDR, LPUART_TX_DMA_CHANNEL, LPUART_TX_DMA_REQUEST);
    DMAMUX_EnableChannel(BT_LPUART_DMAMUX_BASEADDR, LPUART_TX_DMA_CHANNEL);
#endif

    // Initialize the EDMA module
    edma_config_t dma_config;
    EDMA_GetDefaultConfig(&dma_config);
    EDMA_Init(BT_LPUART_DMA_BASEADDR, &dma_config);
    EDMA_CreateHandle(&m_bluetooth_uart.edma_handle, BT_LPUART_DMA_BASEADDR, LPUART_TX_DMA_CHANNEL);

#if defined(FSL_FEATURE_EDMA_HAS_CHANNEL_MUX) && FSL_FEATURE_EDMA_HAS_CHANNEL_MUX
    EDMA_SetChannelMux(EXAMPLE_LPUART_DMA_BASEADDR, LPUART_TX_DMA_CHANNEL, DEMO_LPUART_TX_EDMA_CHANNEL);
#endif

    // Create LPUART DMA handle
    LPUART_TransferCreateHandleEDMA(BLUETOOTH_UART_PORT,
                                    &m_bluetooth_uart.lpuart_edma_handle,
                                    lpuart_edma_transfer_callback,
                                    NULL,
                                    &m_bluetooth_uart.edma_handle,
                                    NULL);

    log_info("UART initialized");
}

 

Any help with this issue will be appreciated. Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,623件の閲覧回数
andyteufel
Contributor III
0 件の賞賛
返信
1 返信
2,623件の閲覧回数
andyteufel
Contributor III
0 件の賞賛
返信