UART Error about the i.MX53_SMD_BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

UART Error about the i.MX53_SMD_BSP

1,182件の閲覧回数
larson
Contributor III

Hello everyone,

 

        I want to use the UART1/2/3/4/5  for my application serial communication, but when i create a serial port in my application, the baudrate is always 9600, when serial port create success, i can see the baud rate is set(use the debug serial port, see the attachment), so why? If somebody know about it, please tell me, thanks! 

Original Attachment has been moved to: SMD_BSP.txt.zip

タグ(2)
0 件の賞賛
返信
4 返答(返信)

978件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,larson,

    By default, UART1/UART2/UART3 are iomuxed in mx53_smd.c :

/* UART1 */

MX53_PAD_CSI0_DAT10__UART1_TXD_MUX,

MX53_PAD_CSI0_DAT11__UART1_RXD_MUX,

/* UART2----used by GPS */

MX53_PAD_PATA_BUFFER_EN__UART2_RXD_MUX,

MX53_PAD_PATA_DMARQ__UART2_TXD_MUX,

/* BT: UART3---used by Bluetooth*/

MX53_PAD_EIM_D24__UART3_TXD_MUX,

MX53_PAD_EIM_D25__UART3_RXD_MUX,

MX53_PAD_EIM_EB3__UART3_RTS,

MX53_PAD_EIM_D23__UART3_CTS,

UART1 is used to be debug UART. so you can't use UART2 & UART3.

/*UART4 & UART5*/

UART4 & UART5 signals are not routed out via i.mx53 pads. From reference manual of i.mx53, they can be iomuxed via CSI0 port or Keypad port:

uart4-uart5-imx53.png

If you want to use them, you should check if their signals are iomuxed via correspongding pads and if iomux settings have been done in bsp file.

Regards,

Weidong


978件の閲覧回数
larson
Contributor III

Hi Weidong,

     Thanks for your help.

     I configuration the UART IO port, and delete the other driver in the BSP, so the UART2/3/4/5 can be used, i test them and can send/recive data, but the baud rate when i create the com port is still 9600, when i use the high baud rate like 38400 to create the com port, the transmission of data will be lost, so do you know what about it?

0 件の賞賛
返信

978件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,larson,

      Please compare your application code with mine, I paste source code that I have used here.

Regards,

Weidong

0 件の賞賛
返信

978件の閲覧回数
larson
Contributor III

Hello Weidong,

        Thanks for your help, i'm work at WINEC700 platform.

     Regards,

     larson

0 件の賞賛
返信