Hi,
I am using u-boot-imx_2013.04 for u-boot-mfgtool.
How to configure u-boot for Parallel NOR operation? When I changed the macro in mx6qsabreauto.h in include/configs/ to
#define CONFIG_SYS_USE_EIMNOR
I got the following error:
| /home/ark7cob/iMX6_Ref/DevelopmentEnvLinuxYocto/Tool.Yocto_CoC_Daisy/build/tmp/work/imx6qsabreauto-poky-linux-gnueabi/u-boot-imx-mfgtool/2013.04-r0/git/drivers/usb/host/ehci-hcd.c:1262: undefined reference to `usb_maxpacket'
| arm-poky-linux-gnueabi-ld.bfd: BFD (GNU Binutils) 2.24 assertion fail /home/ark7cob/iMX6_Ref/DevelopmentEnvLinuxYocto/Tool.Yocto_CoC_Daisy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/binutils-cross/2.24-r0/binutils-2.24/bfd/elf32-arm.c:7696
| arm-poky-linux-gnueabi-ld.bfd: BFD (GNU Binutils) 2.24 assertion fail /home/ark7cob/iMX6_Ref/DevelopmentEnvLinuxYocto/Tool.Yocto_CoC_Daisy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/binutils-cross/2.24-r0/binutils-2.24/bfd/elf32-arm.c:7696
| arm-poky-linux-gnueabi-ld.bfd: BFD (GNU Binutils) 2.24 assertion fail /home/ark7cob/iMX6_Ref/DevelopmentEnvLinuxYocto/Tool.Yocto_CoC_Daisy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/binutils-cross/2.24-r0/binutils-2.24/bfd/elf32-arm.c:7696
| arm-poky-linux-gnueabi-ld.bfd: BFD (GNU Binutils) 2.24 assertion fail /home/ark7cob/iMX6_Ref/DevelopmentEnvLinuxYocto/Tool.Yocto_CoC_Daisy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/binutils-cross/2.24-r0/binutils-2.24/bfd/elf32-arm.c:7696
| arm-poky-linux-gnueabi-ld.bfd: BFD (GNU Binutils) 2.24 assertion fail /home/ark7cob/iMX6_Ref/DevelopmentEnvLinuxYocto/Tool.Yocto_CoC_Daisy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/binutils-cross/2.24-r0/binutils-2.24/bfd/elf32-arm.c:7696
| arm-poky-linux-gnueabi-ld.bfd: BFD (GNU Binutils) 2.24 assertion fail /home/ark7cob/iMX6_Ref/DevelopmentEnvLinuxYocto/Tool.Yocto_CoC_Daisy/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/binutils-cross/2.24-r0/binutils-2.24/bfd/elf32-arm.c:7696
| arm-poky-linux-gnueabi-ld.bfd: error: required section '.rel.plt' not found in the linker script
| arm-poky-linux-gnueabi-ld.bfd: final link failed: Invalid operation
| make: *** [u-boot] Error 1
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/ark7cob/iMX6_Ref/DevelopmentEnvLinuxYocto/Tool.Yocto_CoC_Daisy/build/tmp/work/imx6qsabreauto-poky-linux-gnueabi/u-boot-imx-mfgtool/2013.04-r0/temp/log.do_compile.15429)
NOTE: recipe u-boot-imx-mfgtool-2013.04-r0: task do_compile: Failed
NOTE: Tasks Summary: Attempted 221 tasks of which 220 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
/home/ark7cob/iMX6_Ref/DevelopmentEnvLinuxYocto/Tool.Yocto_CoC_Daisy/sources/poky/meta-fsl-arm/recipes-bsp/u-boot/u-boot-imx-mfgtool_2013.04.bb, do_compile
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
I am using git://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git and imx_v2013.04_3.10.17_1.0.0_ga branch. Please help me to solve this error.
Regards,
Karthikeyan,
+919043955880,
Original Attachment has been moved to: Error.log.zip
Hi Karthikeyan
usb should be disabled from build, as described attached Release Notes
Table 9. Known Issues and Workarounds for i.MX 6Dual/6Quad SABRE-AI:
USB OTG and USB host cannot work after WEIM-NOR or SPI-NOR are
enabled on kernel.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
USB OTG and USB Host are disabled. But still I am getting this error.
I forgot to mention that, Initially i am building the code with CONFIG_SYS_USE_NAND and once the binary is created I am changing the config to CONFIG_SYS_USE_EIMNOR to avoid Yocto fetching the source again which causes my local modification to discard.
Regards,
Karthikeyan,
+919043955880.
seems 3.10.17 mfg tools does not support Parallel NOR configuration, suggest to
move 3.10.31 or last 3.14.28
~igor