U-Boot releases for RIoTboard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

U-Boot releases for RIoTboard

Jump to solution
1,470 Views
Xavier
Contributor III

Hi! I'm currently trying to find a recent version of U-Boot for the RIoTboard. Indeed the one provided in the sources of Android on the Embest website (RIoTboard Development Platform) was released in August 2009 and it seems I'm missing some utilities (usb notably) I need to update U-Boot thanks to a USB stick. Any ideas?

Labels (4)
Tags (2)
0 Kudos
1 Solution
884 Views
fabio_estevam
NXP Employee
NXP Employee

Xavier,

Riotboard is supported in mainline U-boot:

http://git.denx.de/?p=u-boot.git;a=blob;f=board/embest/mx6boards/mx6boards.c;h=f8c746824a7625edb6a36...

So just use the lastest 2015.01 and your Riotboard will work there ;-)

Regards,

Fabio Estevam

View solution in original post

0 Kudos
3 Replies
885 Views
fabio_estevam
NXP Employee
NXP Employee

Xavier,

Riotboard is supported in mainline U-boot:

http://git.denx.de/?p=u-boot.git;a=blob;f=board/embest/mx6boards/mx6boards.c;h=f8c746824a7625edb6a36...

So just use the lastest 2015.01 and your Riotboard will work there ;-)

Regards,

Fabio Estevam

0 Kudos
884 Views
Xavier
Contributor III

My bad... I should've paid more attention. Sorry guys!

0 Kudos
884 Views
SergioSolis
NXP Employee
NXP Employee

Hello Xavier,

I did some lookup on this on google and found that there are a couple of available BSPs here:

http://www.element14.com/community/docs/DOC-68442/l/riotboard-bsp-images-and-tools-download--android...

(check the comments section from that link)

I recommend you to ask in the RIoT board forums too, I'm not sure if they have more recent versions of u-boot.


Have a great day,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------