I'm trying to port U-Boot for an custom I.Mx35 board with only NAND-Flash, the board comes with an RedBoot bootloader.
Is there someone who has any experience with booting from NAND flash?
I have read some I.Mx configurations and I could only find one device booting directly from NAND (Karo - tx25, I.Mx25).
But I'm not sure if this will also work for the I.Mx35?!?
Max
Please refer to app note AN4172 (U-Boot® for i.MX35 Based Designs)
http://cache.freescale.com/files/dsp/doc/app_note/AN4172.pdf
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------