Typical Power Consumption SABRE SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Typical Power Consumption SABRE SDB

989 Views
Jochi119
Contributor II

Hello,

I am working with an i.MX6Q and using the SABRE SDB as my platform.  When looking at the schematics on pg.19 of 25 I see the Current consumption for the power rails on the PF0100.  My question is: SW1A & SW1B (VDDCORE) has a current consumption of 2155mA for the processor, but SYS_4V2 which is supplying power to the entire board has a current draw of only 1001mA for that rail.  It might be a stupid question, but if I total up the current consumption for the board we total 7375mA and right next to it they show "Total system Current Requirements" of 4454mA for SYS_4V2.  How can this be?

Current Consumption.JPG

Labels (1)
0 Kudos
Reply
3 Replies

876 Views
igorpadykov
NXP Employee
NXP Employee

Hi Joseph

typical power consumption data measured on real board is given in

AN4509 i.MX 6Dual/6Quad Power Consumption Measurement

datasheets gives max. theoretical values often not reachable in real applications.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

876 Views
Jochi119
Contributor II

Hey Igor,

I saw this App note, thanks for that. My question would be if you add up all the power under current drawn we get around 7375mA but the schematic only has around 4454mA for total system current requirement. The power supply that comes with the SABRE card also is only 5A.  Where does all the extra power come from?

0 Kudos
Reply

876 Views
igorpadykov
NXP Employee
NXP Employee

Hi Joseph

7375mA is max. available (max. per datasheet), not reachable in real applications.

~igor

0 Kudos
Reply