Two Channel LVDS Display on Sabre SD Board with i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two Channel LVDS Display on Sabre SD Board with i.MX6

2,090 Views
michaellabitzke
Contributor I

Hello together,

I want to drive a Dual-Channel LDSV Display with 1920 x 1200 from Sabre SD Board.

The Sabre SD Board offers me two different LVDS connectors, so I can do a Connection from the board to my Panel using even and odd signals.

How and where can I adjust in the Software (Android), so the i.MX6 generates Dual-Channel LVDS Signal so the odd Signal on LVDS0 and the even Signals on LVDS1?

Thank you very much for any Kind of Support.

Michael

Labels (3)
0 Kudos
Reply
1 Reply

728 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michael

one can try to use kernel parameter ldb=spl0/1, refer to attached Release Notes

p.9, patch and link. Note lcd timings also should be adjusted

iMX6QD How to Add 24-bit LVDS Support in Android

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply