Two Channel LVDS Display on Sabre SD Board with i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two Channel LVDS Display on Sabre SD Board with i.MX6

2,015件の閲覧回数
michaellabitzke
Contributor I

Hello together,

I want to drive a Dual-Channel LDSV Display with 1920 x 1200 from Sabre SD Board.

The Sabre SD Board offers me two different LVDS connectors, so I can do a Connection from the board to my Panel using even and odd signals.

How and where can I adjust in the Software (Android), so the i.MX6 generates Dual-Channel LVDS Signal so the odd Signal on LVDS0 and the even Signals on LVDS1?

Thank you very much for any Kind of Support.

Michael

ラベル(3)
0 件の賞賛
返信
1 返信

653件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Michael

one can try to use kernel parameter ldb=spl0/1, refer to attached Release Notes

p.9, patch and link. Note lcd timings also should be adjusted

iMX6QD How to Add 24-bit LVDS Support in Android

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信