[Troubles] ltib failed build on dbus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Troubles] ltib failed build on dbus

1,406件の閲覧回数
marcobari
Contributor I

Hi,

I'm trying to build linux kernel on Ubuntu 9.04 for iMX6 but build failed on dbus.

How I can resolve the problem?

Thanks in advance

Marco

/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/../lib/gcc/arm-fsl-linux-gnueabi/4.6.2/../../../../arm-fsl-linux-gnueabi/bin/ld: cannot find -lX11

collect2: ld returned 1 exit status

make[2]: *** [dbus-launch] Error 1

make[2]: *** Waiting for unfinished jobs....

gcc -ffunction-sections -fdata-sections -g -O2 -Wall -Wchar-subscripts -Wmissing-declarations -Wmissing-prototypes -Wnested-externs -Wpointer-arith -Wcast-align -Wsign-compare -Wdeclaration-after-statement -fno-common -o .libs/dbus-send dbus-print-message.o dbus-send.o  ../dbus/.libs/libdbus-1.so

gcc -ffunction-sections -fdata-sections -g -O2 -Wall -Wchar-subscripts -Wmissing-declarations -Wmissing-prototypes -Wnested-externs -Wpointer-arith -Wcast-align -Wsign-compare -Wdeclaration-after-statement -fno-common -o .libs/dbus-uuidgen dbus-uuidgen.o  ../dbus/.libs/libdbus-1.so

gcc -ffunction-sections -fdata-sections -g -O2 -Wall -Wchar-subscripts -Wmissing-declarations -Wmissing-prototypes -Wnested-externs -Wpointer-arith -Wcast-align -Wsign-compare -Wdeclaration-after-statement -fno-common -o .libs/dbus-monitor dbus-monitor.o dbus-print-message.o  ../dbus/.libs/libdbus-1.so

creating dbus-send

creating dbus-uuidgen

creating dbus-monitor

make[2]: Leaving directory `/home/marco/ltib/rpm/BUILD/dbus-1.2.3/tools'

make[1]: *** [all-recursive] Error 1

make[1]: Leaving directory `/home/marco/ltib/rpm/BUILD/dbus-1.2.3'

make: *** [all] Error 2

error: Bad exit status from /home/marco/ltib/tmp/rpm-tmp.21247 (%build)

RPM build errors:

    Bad exit status from /home/marco/ltib/tmp/rpm-tmp.21247 (%build)

Build time for dbus: 67 seconds

Failed building dbus

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Thu May 23 10:42:15 2013

Ended:   Thu May 23 10:45:41 2013

Elapsed: 206 seconds

These packages failed to build:

dbus

Build Failed


0 件の賞賛
5 返答(返信)

762件の閲覧回数
LeonardoSandova
Specialist I

Strange, it is complaining that X11 library is missing, but I just compiled the package without this library and worked. On your setup, please add libX11 on the  LTIB menu and run build again.

Leo

762件の閲覧回数
marcobari
Contributor I

Hi Gonzalez, thank you for your reply.

I have builded linux kernel successfully, tnks.

I have another question, I have only rpm package manager, but I don't find rpm repository.

I need to install openvpn on iMX6, where I can find rmp for arm?


0 件の賞賛

762件の閲覧回数
YixingKong
Senior Contributor IV

Hi Marco, I am going to close your dicussion since it seems your issue has been resolved. If you have other question please feel free to create another discussion.

Thanks,

Yixing

0 件の賞賛

762件の閲覧回数
LeonardoSandova
Specialist I

The best way to install a new package is through LTIB. Place the tarball on /opt/freescale/pkgs and create a .spec for the package (under ltib/dist/..) , then use the ltib script to prepare (='untar and patch'), scbuild (= configure and compile) and scinstall (create the rpm package) and scdeploy (install that rmp on rootfs).

Leo

762件の閲覧回数
marcobari
Contributor I

Hi Leo,

your suggestion was very useful.

Thanks
Marco

0 件の賞賛