I'm trying to load and run the "hello world" example on my IMX8MMEVK board by following this page:
https://www.nxp.com/document/guide/get-started-with-the-i-mx-8m-mini-evkb:GS-iMX-8M-Mini-EVK
I have flashed the latest stock Linux BSP to EMMC and I have built my own stock image and flashed the SD card with that. I can see that the examples are there on the SD card. I get the following results on the Uboot console:
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from MMC1
NOTICE: BL31: v2.6(release):lf-5.15.32-2.0.0-0-gc6a19b1a3
NOTICE: BL31: Built : 06:37:22, Jun 7 2022
U-Boot 2022.04-lf_v2022.04+g1c881f4da8 (Jun 07 2022 - 05:16:02 +0000)
CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 39C
Reset cause: POR
Model: NXP i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
Core: 169 devices, 30 uclasses, devicetree: separate
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment
[*]-Video Link 0 (1920 x 1080)
[0] lcdif@32e00000, video
[1] mipi_dsi@32e10000, video_bridge
[2] adv7535@3d, panel
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated
BuildInfo:
- ATF c6a19b1
switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net: eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
u-boot=> fatload mmc 0:1 0x7e0000 imx8mm_m4_TCM_hello_world.bin
Couldn't find partition mmc 0:1
Can't set block device
u-boot=> fatload mmc 1:1 0x7e0000 imx8mm_m4_TCM_hello_world.bin
** Reading file would overwrite reserved memory **
Failed to load 'imx8mm_m4_TCM_hello_world.bin'
u-boot=> fatload mmc 1:1 0x800000 imx8mm_m4_TCM_hello_world.bin
** Reading file would overwrite reserved memory **
Failed to load 'imx8mm_m4_TCM_hello_world.bin'
u-boot=>
What am I missing or doing wrong?
解決済! 解決策の投稿を見る。
Hello,
Please try with the following commands:
> fatload mmc 1:1 0x48000000 imx8mm_m4_TCM_hello_world.bin
> cp.b 0x48000000 0x7e0000 0x20000
> dcache flush
> bootaux 0x7e0000
Best regards,
Aldo.
Hello,
Please try with the following commands:
> fatload mmc 1:1 0x48000000 imx8mm_m4_TCM_hello_world.bin
> cp.b 0x48000000 0x7e0000 0x20000
> dcache flush
> bootaux 0x7e0000
Best regards,
Aldo.
Thanks so much! Now I have to figure out what I did. If you have any other pearls of wisdom feel free to impart. Thanks again.
Hello,
Sorry for not being clear, please see below for a more detailed response:
The command you have used is no longer correct, this is because u-boot from >= L5.4.24 checks if the load address is in a reserved area of memory for u-boot or not.
So now we need to fatload the bin to DDR (0x48000000) by using the following command:
> fatload mmc 1:1 0x48000000 imx8mm_m4_TCM_hello_world.bin
Next will be copying the binary from that location to TCM (0x7e0000)
> cp.b 0x48000000 0x7e0000 0x20000
Finally we flush dcache and boot the auxiliary core (Cortex-M4)
> dcache flush
> bootaux 0x7e0000
Best regards,
Aldo.