Hi,
I could get temperature via SCFW API (sc_misc_get_temp) . But, I would like to confirm a few points.
Q1. I was getting following result with MEK and linux bsp.
thermal_zone0 is CPU temperature. thermal_zone1 is DDR controller temperature. is it right?
If yes, These temperature difference of 25°C between CPU and DDR controller. Is this reasonable?
root@imx8qxpmek:~# cat /sys/class/thermal/thermal_zone0/temp
45000root@imx8qxpmek:~# cat /sys/class/thermal/thermal_zone1/temp
70000
Q2. Linux BSP is able to chose SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2 for resource parameter.
Which module's temperature can I get by specifying these resources?
Copy from linux_4.14.98_2.3.0_ga/drivers/thermal/imx_sc_thermal.c
Best Regards,
Kazuma Sasaki.
已解决! 转到解答。
Hi Kazuma
1. > ..difference of 25°C between CPU and DDR controller. Is this reasonable?
DRC (DDR) temperature sensor readings are wrong due to erratum ERR050055
https://www.nxp.com/docs/en/errata/IMX8X_0N95W.pdf
2. SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2 are PMIC temperature
sensors described in PF8100 datasheet
https://www.nxp.com/docs/en/data-sheet/PF8100_PF8200.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kazuma
1. > ..difference of 25°C between CPU and DDR controller. Is this reasonable?
DRC (DDR) temperature sensor readings are wrong due to erratum ERR050055
https://www.nxp.com/docs/en/errata/IMX8X_0N95W.pdf
2. SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2 are PMIC temperature
sensors described in PF8100 datasheet
https://www.nxp.com/docs/en/data-sheet/PF8100_PF8200.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Kazuma
> What is different SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2
these are PMIC temperature sensors, described in PF8100 datasheet
https://www.nxp.com/docs/en/data-sheet/PF8100_PF8200.pdf
Best regards
igor
Hi Igor,
I am sorry for not explaining enough.
PF8100 has ten temperature sensors. Which sensor temperature can be acquired by selecting SC_R_PMIC_0?
Also, I would to know about SC_R_PMIC_1 and SC_R_PMIC_2.
Best Regards,
Kazuma Sasaki.
Hi Igor,
Please let me confirm one thing.
What is the difference between SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2?
Before you told me that these settings will be return the temperature of center of die.
How should I use these settings properly?
MEK has one PMIC. At that case, can we select SC_R_PMIC_1 and SC_R_PMIC_2?
Best Regards,
Kazuma Sasaki.