Thermal sensor of iMX8X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Thermal sensor of iMX8X

ソリューションへジャンプ
7,252件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi,

I could get temperature via SCFW API (sc_misc_get_temp) . But, I would like to confirm a few points.

pastedImage_3.png

Q1. I was getting following result with MEK and linux bsp.

thermal_zone0 is CPU temperature. thermal_zone1 is DDR controller temperature. is it right?

If yes, These temperature difference of 25°C between CPU and DDR controller. Is this reasonable?

root@imx8qxpmek:~# cat /sys/class/thermal/thermal_zone0/temp
45000

root@imx8qxpmek:~# cat /sys/class/thermal/thermal_zone1/temp
70000

Q2. Linux BSP is able to chose SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2 for resource parameter.

Which module's temperature can I get by specifying these resources?

Copy from linux_4.14.98_2.3.0_ga/drivers/thermal/imx_sc_thermal.c

pastedImage_1.png

pastedImage_4.png

Best Regards,

Kazuma Sasaki.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
7,117件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

1. > ..difference of 25°C between CPU and DDR controller. Is this reasonable?

DRC (DDR) temperature sensor readings are wrong due to erratum ERR050055
https://www.nxp.com/docs/en/errata/IMX8X_0N95W.pdf

2. SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2 are PMIC temperature
sensors described in PF8100 datasheet
https://www.nxp.com/docs/en/data-sheet/PF8100_PF8200.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
7,117件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

SC_R_PMIC_0 - Center of die

SC_R_PMIC_1 - Vicinity of SW1

SC_R_PMIC_2 - Vicinity of SW2

Best regards
igor

7,117件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Dear Igor,

I got it. thanks.

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信
7,118件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

1. > ..difference of 25°C between CPU and DDR controller. Is this reasonable?

DRC (DDR) temperature sensor readings are wrong due to erratum ERR050055
https://www.nxp.com/docs/en/errata/IMX8X_0N95W.pdf

2. SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2 are PMIC temperature
sensors described in PF8100 datasheet
https://www.nxp.com/docs/en/data-sheet/PF8100_PF8200.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
7,117件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

Thank you for your support.

Let me confirm once again. What is different SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2?

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信
7,117件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Kazuma

 

> What is different SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2

 

these are PMIC temperature sensors, described in PF8100 datasheet
https://www.nxp.com/docs/en/data-sheet/PF8100_PF8200.pdf

 

Best regards
igor

0 件の賞賛
返信
7,117件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

I am sorry for not explaining enough.

PF8100 has ten temperature sensors. Which sensor temperature can be acquired by selecting SC_R_PMIC_0?

Also, I would to know about SC_R_PMIC_1 and SC_R_PMIC_2.

pastedImage_2.png

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信
7,117件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

>. Which sensor temperature can be acquired by selecting SC_R_PMIC_0?

1. Center of die

and so on.

Best regards
igor

0 件の賞賛
返信
7,117件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

Please let me confirm one thing.

What is the difference between SC_R_PMIC_0, SC_R_PMIC_1 and SC_R_PMIC_2?

Before you told me that these settings will be return the temperature of center of die.

How should I use these settings properly?

MEK has one PMIC. At that case, can we select SC_R_PMIC_1 and SC_R_PMIC_2?

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信
7,117件の閲覧回数
Kazuma_Sasaki
Senior Contributor I

Hi Igor,

I appreciate your support. I got it.

Best Regards,

Kazuma Sasaki.

0 件の賞賛
返信