The A0 version of ixm8qm_mek ADAPTS to the current code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The A0 version of ixm8qm_mek ADAPTS to the current code

442 Views
dhty2015
Contributor II

The A0 version of imx8qm_mek is now used, but the B0 version is now available by default.

Now uboot cannot boot directly.Even if you compile it yourself, the bl31.bin and scfw_semc.bin files don't match (and there may be others), and there is no way to provide these outdated but necessary files directly?

0 Kudos
Reply
1 Reply

405 Views
igorpadykov
NXP Employee
NXP Employee

Hi yuelin

unfortunately i.MX8QM A0 is not more supported, one can try to

obtain its images through local marketing office or with professional services.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply