Target detected as "unknown device" -imx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Target detected as "unknown device" -imx6

498 次查看
rajesh7989
Contributor I

Hi,

   I am using MfgtTool2 to flash a target. When the target enters boot mode windows recognizes as a unknown device and the Mfgtool2 shows "No device connected".

Can someone help me on this issue. Thanks in advance.

标签 (1)
0 项奖励
1 回复

369 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rajesh

some problems may be with Windows 7 64 bits or USB 3.0 controller

(enumeration problem may be related to USB3.0 controllers (XHCI) and the

associated driver. Was found that the command sequence for enumeration on a

XHCI controller is different from enumeration on an EHCI controller). 

One can try other PC using Windows XP or 32bit Windows 7 or disable USB 3.0.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励